STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Minor error in CMSIS-mandated device headers (yes, in Cube)

Posted on April 26, 2017 at 12:22[STM32Cube_FW_F4_V1.15.0]\Drivers\CMSIS\Device\ST\STM32F4xx\Include\stm32f4*.h:#define USART_CR1_TXEIE               USART_CR1_TXEIE_Msk                      /*!<PE Interrupt Enable                    */The comment i...

STM32F103 SPI configuration troubles

Posted on April 24, 2017 at 18:18 Hi all, I'm having hard times in configuring SPI communication with a M95128 eeprom; I'm using SPI1 on a STM32F103 mcu, with following connection scheme: PA.04 -> ~S (CS) PA.05 -> C (CLK) PA.06 -> Q (...

How to programme a powerstep01?

Posted on April 25, 2017 at 10:09Anybody who can teach me how to use a powerstep01 to drive the step motor?I have the demo boards and the powerstep01 works well with the demos and the download software from st.com.Now, i want to use another MCU (low...

Lin SS by Associate
  • 1122 Views
  • 1 replies
  • 0 kudos

Resolved! I need help

Posted on April 26, 2017 at 10:44Hi,I am newbie in System Workshop for STM32. I tried write simple example - LED blink. It works fine.Now I want to test the same program, but with a timer interrupt.In file ''stm32f4xx_hal_conf.h''  I enable HAL_TIM_...

0690X00000602S7QAI.bmp 0690X00000602SLQAY.bmp 0690X00000602SaQAI.bmp
Peko by Associate III
  • 1598 Views
  • 2 replies
  • 0 kudos

Resolved! Nucleo L432KC bootloader via UART failed

Posted on April 25, 2017 at 10:23Hi, I met a problem using bootloader on pc to wirte program into STM32L432KC via UART.Here is the process I did :1,I connect D1/Tx and D0/RX(PA9 and PA10 of STM32L432KC) to CH340 USB to UART board, 5V Vin and GND. US...

0690X00000605tnQAA.png 0690X00000605w5QAA.png 0690X00000606r0QAA.png
Yu LU by Associate II
  • 2937 Views
  • 4 replies
  • 0 kudos

RTL 000.0 TCP-ERR:Send, Socket 1 reentrant callback

Posted on April 26, 2017 at 09:44hi,I  work on rtl-tcp over ppp protocol. First gsm modüle is given IP by AT commands and then is connected ethernet over ppp protocol.  At software , tcp socket is opened and tcp_send function is worked over ppp . RT...

ali2399 by Associate II
  • 748 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.