STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SW4STM32 + STM32F411E Disco

Posted on March 21, 2017 at 12:47When I try to run and debug a project with SW4STM32-Eclipse I get the following error message:Error in final launch sequenceFailed to execute MI command:-exec-runError message from debugger back end:Don't know how to...

Luca R by Associate II
  • 969 Views
  • 3 replies
  • 0 kudos

STM32F030: Interrupt remaping to RAM

Posted on April 28, 2017 at 04:33Hi,I am developing bootloader for STM32F030ccT6 to upgrade my Main Application through OTA. There are two application within my controller flash one is BOOTLOADER( @ 0x08000000) and other is Main Application( @ 0x080...

STM32F103 SPI question

Posted on April 28, 2017 at 12:57This is the first time I need SPI, and there are two things that are still unclear to me:1) I understand that to receive from a slave, I need to send something - maybe zeros?So if I have a chip that takes register ad...

Resolved! CubeMX 4.20.0 Problem

Posted on March 14, 2017 at 08:18I think the new issue seems to have a problem with source generation.When choosing the HSE, create the source as follows :  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;To operate ...

Resolved! HSE Bypass Clock Source w/CubeMX and Nucleo 303ZE fails

Posted on March 27, 2017 at 01:42Possible bug in CubeMX 4.20.0?Using Nucleo 303ZE board, and Atollic 7.1.1Build dead simple default project, except in RCC, set High Speed Clock to 'BYPASS Clock Source', and select HSE as input to PLL.In main.c you'l...

Changing clock source from HSE to HSI

Posted on August 26, 2015 at 08:16Hi Please refer below code to change clock source from external HSE to internal HSI /* Enable HSE Oscillator and activate PLL with HSE as source */#if 0 // Choose External Crystal (HSE) As Source RCC_OscInitStruct.O...

sangamesh by Associate II
  • 3329 Views
  • 5 replies
  • 0 kudos

HAL Timer PWM DMA Completion

Posted on April 27, 2017 at 23:34 I have an app running on F303 where i build an waveform buffer of PWM widths (CCR1) and then periodically send the waveform using HAL_TIM_PWM_Start_DMA. Project is CUBE generated.It all works find, resending the ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.