STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L072: PWM Output with HAL

Posted on May 20, 2017 at 14:34Hello everybody!I cannot find whats missing in my timer initialisation: TIM3_CH2 interrupt is generated correctly (as the callback function is executed and a led on a generic GPIO of the STM32 Demo Board is driven by c...

davide by Associate II
  • 1942 Views
  • 2 replies
  • 0 kudos

DecaWave USB Driver for Linux (LabVIEW using RoboRIO)

Posted on May 22, 2017 at 18:55Hi,I am working on an evaluation project using the DecaWave Trek1000 which points me to the V1.4.0 Virtual Com port driver for Window which works great on my Windows 10 PC.  If you are familiar with the DecaWave I am u...

Resolved! UART Framing Error on STM32F1

Posted on May 19, 2017 at 14:32Hi,I have an STM32F1 and am running the UART printf example from the standard peripheral library. I've modified the code to allow me to use USART3 (I'm using a custom pcba and only USART3 is wired to a connector mounte...

0690X00000603aRQAQ.jpg

TIM1 to trigger ADC conversion

Posted on May 21, 2017 at 17:55Hi to everyone, I apologize for the umpteenth discussion on this topic.I have some questions about Timer in general to which I did not found good answers:1- I would like to use TIM1_CH1 to start ADC conversion but from...

Resolved! Cube and JTAG/SWD

Posted on May 22, 2017 at 16:07Hello,the pinout view of Cube is good for planning pin assignment. However I don't see an item for SWD/JTAG to reserve the needed pins.  Do I miss something? Otherwise Cube should get entries for JTAG/SWD.

STM32F429IGT SDRAM Read/Write

Posted on May 22, 2017 at 14:44Hi all,I've got a board with IS45S16400J SDRAM connected to MCU, FMC bank 2. I'm entering data via UART and write it to SDRAM, then I'm reading it and sending back data.Received data looks kinda strange, the first 8 by...

USB HOST

Posted on May 20, 2017 at 04:11Hi:Where is download usb host the firmware library?I want use it to do usb host(class 06h image).Help me,Please.

li chao by Associate
  • 1004 Views
  • 1 replies
  • 0 kudos

STM32F4 USART issue

Posted on May 22, 2017 at 01:33Hello,I've been trying to send data by uart from stm32f429i board to computer through usb. I learned from the datasheet that two pins - PA9 -tx and PA9-rx are connected to ST-LINK programmer so it seemed possible. I up...

Resolved! STM32F746 Disco HardFault

Posted on April 30, 2017 at 15:09Hi,Creating a EmWin application based on a STM32F746 Disco, using OpenSTM32. I toke the STemWin example application as a starting point. Occasionally (once every 1-3 hours of operation) I'm running into a Hard Fault ...

paul2 by Senior
  • 3028 Views
  • 9 replies
  • 0 kudos

Regarding the CAN interface with STM32L476RG

Posted on May 22, 2017 at 12:14Hi,I am usingthe STM 32l476RG . I want to interface 2 same controllers with CAN protocol. So as there was no example for the Eval_board for this controller can u help me out what the set up with MCP2551(CAN transceiver...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.