Development board needed
Posted on June 05, 2017 at 09:46Need a development board for STM32L4A6xG I couldnt find it folks do help me out!
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on June 05, 2017 at 09:46Need a development board for STM32L4A6xG I couldnt find it folks do help me out!
Posted on April 12, 2017 at 17:23I just started with SensorTile develpment. Got the STEVAL-STLCX01V1 in house and have downloaded firmware en.stsw-stlkt01.zip.Got it build success using IAR. As I gone through release doc, it support 3 versions of ...
Posted on June 08, 2017 at 12:30 In my application, I use 8 data bits and odd parity in serial communication (so, it is a 9 bit wordlength). During reception, I found that a variable which was contiguous, but outside the receive buffer, was be...
Posted on June 08, 2017 at 11:09I found the library x-cube-smbus, but it is support only the STM32F0 and STM32F3. And in the example in the file readme.txt it is written that: '- This example has been tested with STM32F3-Discovery boards and can be ...
Posted on June 02, 2017 at 07:32Hai, I am using Stm32f103vbt6 micro controller, I have some issue with interfacing the I2C EEPROM. eeprom is at24cm02. its has only one address pin. In code 'I2C_Send7bitAddress ' this line has sussefully send, My add...
Posted on June 08, 2017 at 09:03 When exporting the GPDSC project output for an STM32F103C8T6 it will contain a files referencing the #include 'core_cm8.h': In file included from /home/mm/STM32-workspace/pocs/Drivers/CMSIS/Device/ST/STM32F...
Posted on June 07, 2017 at 16:01I need a STM32 microcontroller with HDLC interface. Could someone help me to find it?thanks
Posted on June 08, 2017 at 06:10Hi, I am using STM32F103VBT6 micro controller, i have done a RTC code for date and time,But in that, I need to do a interrupt for every 1 minute. Is it possible to do?I have done some code, for interrupt .but its not ...
Posted on June 06, 2017 at 15:33Hi, want to build a 'uart daisy chain' with several (up to 200) STM32 MCUs by connecting TxD of uart number n to RxD of uart number n+1 (1-wire connection). To perform Initial addressing Job I'm thinking to do it like...
Posted on June 07, 2017 at 22:54Thank you for your patronage. I'm Japanese. I want to use Interrupt Service Routine(ISR) as shown in the picture below. So I want to use HAL_HRTIM_IRQHandler.I wrote the program as shown below, but I got an error. #hr...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.