STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How fast can I counter using external interrupt?

Posted on June 28, 2017 at 13:21Hi everyoneI'm usging STM32F103VE @72MhzI wonder how fast can I counter using external interrupt?These days I try to count clock signal by EXTI. ( clock signal is 10 Mhz) Is it possible?If impossible then, what is lim...

Shin KS by Associate
  • 1096 Views
  • 1 replies
  • 0 kudos

spi ,i2c,uart interface with stm32vl discovery board

Posted on June 28, 2017 at 13:47hi i am new to stm32. i have purchased stm32vl discovery board recently. i would like to interface 2 UARTS ,2 spi and one i2c peripherals together with the board .how can i do it using interrupts can any one help me o...

Bug in USB CDC Class Init/Deinit

Posted on June 26, 2017 at 04:04I plug in my CubeMX generated USB CDC class implementation into a PC host and CDC_Init_FS gets called as expectedWhen I unplug, I expect that CDC_DeInit_FS be called so I can take the link down but it doesn't.When I p...

Programming the STM32L152

Posted on June 26, 2017 at 21:52Hello everybody!This is the most basic question a guy who gets involved with microcontrollers can ask.I want to replicate an open source project. The code is provided as well. The project used the STM32L152.I found th...

nick st by Associate
  • 1162 Views
  • 1 replies
  • 0 kudos

STM32F0 irda - Can't receive SIR Data

Posted on June 28, 2017 at 13:15Hi, I am trying to get data from IrDA SIR mode.I setup that USART Port 2 is sending IrDA packet and USART Port 1 is receiving ( it similar to loop-back, wired USART2 TX and USART RX )I can see the irda wave form on US...

stemwin help

Posted on June 28, 2017 at 11:22hi dear i have a problem with the stemwin i want the source code or librey off this functions IMAGE_Handle IMAGE_CreateEx (); IMAGE_Handle IMAGE_CreateUser (); IMAGE_Handle IMAGE_CreateIndirect(); void IMAGE_Callback(...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.