STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bug in \STM32Cube_FW_F1_V1.6.0\STM3210C_EVAL

Posted on July 18, 2017 at 17:04Hi I have built the project STM32Cube_FW_F1_V1.6.0\Projects\STM3210C_EVAL\Applications\FatFs\FatFs_uSD, but he was off with a bug in FatFs study showed that when the functionsBSP_SD_WriteBlocks uint8_t(uint32_t *pData...

STM32F103 SPI->SR TXE bits always set

Posted on July 18, 2017 at 10:28Hi I'm using the SPI module in the STM32F103. I'have a problem. I set the SPI Module and SPI is working. But ? have a problem. When I load a data into the SPIx->DR register, the TXE bit is always set.  The data is bei...

LWIP_IAP: Where is the Fs directory?

Posted on July 18, 2017 at 16:25Hi,  I would like to understand and implement the LWIP_IAP using the HTTP method. But there's no Fs directory with the html pages used to generate the fsdata.c file. How can I get it? Ari.

Asantos by Senior
  • 645 Views
  • 0 replies
  • 0 kudos

STM32F04xx - I2C communication

Posted on July 18, 2017 at 15:53Hello guys, I have problem with reading CPUID base register. I am beginer with STM32, be patient please.My code seq. look like this: I am using soft. I2C from ATMEGA 1280START I2C   write slave adress for write (0x7C)...

STM32L073 flash problem

Posted on July 18, 2017 at 15:07I'm facing some problems while flashing a Release version image into a STM32L073 MCU. The strange thing is thatthis happens only when the size of the binary image to flash is near the one of the Flash Bank 0 size (abo...

Timers options in STM32L

Posted on July 12, 2017 at 23:16Hello engineers,I would like to ask you about Timer possibilities. I do not have much experiences so please be patient. But back to my question, i want to trigger one Timer from external source, wait setted time (vari...

Bluetooth firmware update

Posted on July 18, 2017 at 11:00Hi all,For a project we have to update the firmware of the STM32F469xx over the air by a Bluetooth connectionwith a transmitter (can that be a smart phone?) and receiver on the microcontroller device part.In an articl...

Max Veen by Associate II
  • 704 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.