STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC reading are not constant

Posted on July 20, 2017 at 12:26Hello There,I am using STM3F4 discovery board. I am able to print the ADC value on display. I am using PA0 as ADC i/p. The value is constant 4095 if I connect to 3V from board. If I connect PA0(ADC i/p) to my external...

Exti stop working after jumping to the new firmware stm32L4

Posted on March 31, 2017 at 21:28 http://electronics.stackexchange.com/questions/295904/exti-stop-working-after-jumping-to-the-new-firmware-stm32l4 Hi I am new here ,I am working on an application on stm32l4 microcontroller , the idea is w...

raed by Associate II
  • 5399 Views
  • 16 replies
  • 0 kudos

Resolved! I2C Troubleshooting without an oscilloscope

Posted on July 20, 2017 at 22:52Hello everyone,I recently got myself a little nucleo compatible http://www.waveshare.com/w/upload/3/3a/Accessory-Shield-Schematic.pdf that comes with at I2C Temperature sensor http://www.nxp.com/docs/en/data-sheet/LM7...

stm32f103 I2C 1602 lcd, helpme please

Posted on July 20, 2017 at 18:06I am learning to program in C ++ with the stm32f103, I am trying to connect the stm32f103 with a 1602 LCD through I2C, could someone help me with an example code?

STM32CubeF0 1.8.0 Smart Card Problem

Posted on July 20, 2017 at 00:44I start a new project with smart card function generated by CubeMX with STM32F072RB. The smart card circuit is the same as previous project.  And I have no problem with smart card function in previous project.  I comp...

mtien888 by Associate II
  • 1347 Views
  • 2 replies
  • 0 kudos

Bug on HAL_CAN_ConfigFilter for stm32f105 CubeMX

Posted on February 16, 2016 at 12:10When you set the filters for can2, software try to set the registers at base 0x4006800 + 0x200 instead of  0x4006400 + 0x200.Using handle hcan its correct ?  MODIFY_REG(hcan->Instance->FMR                         ...

Marco1 by Associate II
  • 2722 Views
  • 6 replies
  • 0 kudos

spi, stm32f7

Posted on September 07, 2016 at 14:46 Hello, I have a problem with SPI communication for stm32f746-discovery board. I didnt read any value, and when I looked NSS pin is not moving. Only clock is running. SPI is in receive mode only. Function hw_...

bks by Associate
  • 1559 Views
  • 2 replies
  • 0 kudos

32F746GDISCOVERY Arduino Connector Pinout

Posted on March 22, 2016 at 12:33Hi, is it possible that the arduino connector pinout in documentation and Altium schematic has some errors? e.g. ARD_D10 and ARD_D5 seems to be false. ARD_D5 is PI0  and not PA8 best regards

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.