STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7CubeMX FMC library issue

Posted on July 25, 2017 at 00:03I am trying to use the FMC library to access a Toshiba TC58NVG0S3HTA00 NAND memory device. The ALE line is the wrong sense. It is normally high and goes low when loading an address. I can't find anyone with this probl...

STM32 SPI DMA Timings

Posted on February 13, 2017 at 16:38Hello all,I'm trying to setup the STM32L432 MCU for SPI communication (24 MHz, 16 bit data size, master transmit only), using DMA.The slave device is a 32 channel amplifier chip. I need to send a specific string o...

PWM

Posted on July 24, 2017 at 22:58How can I generate 360 degree out of phase center-aligned PWM waveform (modified sine wave) on two pins with STM32F103?

STM32 DMA EXAMPLE

Posted on July 24, 2017 at 18:42HELLO,                I am currently working with STM32F100C4 controller DMA operation,but its seems little confusing to me... if anyone has any code example of it please share. Thanks.

stm32F4 FPU Question

Posted on July 24, 2017 at 17:01Hello,i am trying to work with the fpu of the stm32f469-Disco and got some questions...i am on ac6 systemworkbench/win7/so far i can compile and run my app that uses float math...when i look at the disassmbly it looks...

0690X00000607fUQAQ.png 0690X00000607evQAA.png

Ethernet and TFT LCD with an STM32F746IGT6 LQPF176

Posted on July 17, 2017 at 10:33I want to build a application with a an STM32F746IGT6 LQPF176 with Ethernet and TFT LCD.I started with CubeMX for checking if this configuration is possible.When I enable:- LTDC Display Type: RGB888 (24bits)- ETH Mode...

Ethernet etiquette ! Closing ?

Posted on July 24, 2017 at 02:30I am new to ethernet, finally running on my private PCB.I have an industrial scenario, many slaves talking to the master over can-bus, then the master is talking to a server on the cloud.there will be several masters ...

T J by Lead
  • 1382 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.