STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F303K8 DAC problem

Posted on July 14, 2017 at 13:38The original post was too long to process during our migration. Please click on the attachment to read the original post.

Rad Rad by Associate II
  • 2689 Views
  • 4 replies
  • 0 kudos

STM32L476VG User_Usb

Posted on August 22, 2017 at 13:14Hi sir I'm working on  STM32L476VG board for this i want to do communication with User USB as Device and PC as host could you please help me for driver  to access user USB or tell me what i have to do to access user...

STLINK Utility V4.0.0 problem

Posted on August 09, 2017 at 04:04Hi, I am currently playing with micropython on NUCLEO-L476RG and get it flashed and working using STLINK Utility V3.9.0But then when I update to STLINK Utility V4.0.0, using the same exact .HEX files, It stop workin...

Why it always takes 12 clock cycle while using the STLINK to trace single instruction's execution time?(about dual-issue, St-link and Cortex-M7 pipeline)

Posted on August 22, 2017 at 12:25The device is STM32F746NG-DISCO, and I measure the execution time of single instruction by this ways:int a=0; int b=255;while(b--) { a++; }make breakpoint and watch the value of States. And by this, I found that for...

0690X00000607zUQAQ.png 0690X00000607zAQAQ.png 0690X00000607wvQAA.png

stm32f042f6 spi doesn't work with HSI as PLL source

Posted on August 20, 2017 at 21:37Hello! I'm using spi peripheral on STM32f042f6p6 and faced with strange situation: spi works only if system clock is PLL and HSE is PLL source. I have tried HSI, HSI48, with them spi does not work at all: neither tr...

EvgenS Po by Associate II
  • 2084 Views
  • 4 replies
  • 0 kudos

STM32F4 HAL for TIM PWM and Encoder Input

Posted on November 09, 2015 at 05:13Hello, I am trying to use the STM32F4 HAL Drivers to read a 50 Hz PWM input signal and an A quad B encoder signal on an STM32F4 Discovery board, but the TIMx_CNT register is NOT incrementing on the external trigg...

SPI DMA transmit during interrupt

Posted on August 22, 2017 at 10:37Hello!I am implementing a state machine which is driven by interrupts on the STM32F437IIT6.The interrupts occur as a result of using the HAL_SPI_Transmit_DMA() function.While testing my program i have noticed that w...

YuriCh by Associate II
  • 813 Views
  • 0 replies
  • 0 kudos

how to get more info after watchdog reset

Posted on August 22, 2017 at 09:46We are using quite a few stm32 MCUs from 401 to 439, and our program becomes more and more complicated. In order to avoid possible deadloop, we have used watchdog to rescue the system, basically it is working well n...

jeff23 by Associate II
  • 928 Views
  • 0 replies
  • 0 kudos

Cannot restart application

Posted on August 22, 2017 at 09:07I need to restart my application without starting the bootloader or any reset (Watchdog, Soft-Reset,....).Processor: SMT32F207Bootloader start address is 0x08000000, application is starting at 0x08020000.The recomme...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.