HAL_GetUID
Posted on October 05, 2017 at 09:31When compiling using the HAL library STM32Cube_FW_F4_V1.16.0 I am getting an error that UID_BASE is not defined.Can someone point me out if I am missing a header file or declaration?
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on October 05, 2017 at 09:31When compiling using the HAL library STM32Cube_FW_F4_V1.16.0 I am getting an error that UID_BASE is not defined.Can someone point me out if I am missing a header file or declaration?
Posted on March 10, 2018 at 08:38 The follow code snippet is generated in sd_diskio.c by CubeMX (4.0) when using FreeRTOS (STM32Cube_FW_F7_V1.9.0): /** * @brief Gets Disk Status * @param lun : not used * @retval DSTATUS: Operation status *...
Posted on March 09, 2018 at 16:12Where are any STM32Cube example projects for the B-L475E-IOT01A board? I can find the generated projects for example BLE/HeartRate and P2P_LedButton. But how were these generated? Isn't the whole point of using...
Posted on March 09, 2018 at 16:21We are working on a motor controller and started with a evaluation board that uses the STM32F031. Unfortunately we have utilized over 80% of the flash and 90% of the RAM, so going forward with the STM32F031 is a bit ...
Posted on March 08, 2018 at 16:28Hi, I've a problem with the jitter of my program on STM32L476.First of all, I'm introduced you my project.A signal TLL with a frequency of 1KHz to 50 KHz must be multiplied by a sinusoide or square analogique signal ...
Posted on March 09, 2018 at 16:27Has anyone replaced the shunt resistors with a isolated hall-effect current sensor?We need isolation for safety, but there is concern of introducing phase lag in the current signals.#iso-shunt-current #isolated-curre...
Posted on March 07, 2018 at 22:25HiI use stm32f407 to communicat with rs485.I use DMA to transmit data. For controllig dirction pin, I check the USART_FLAG_TC. Whet it is set, I will push Dirction pin low and clear the USART_FLAG_TC by writing with ...
Posted on March 08, 2018 at 04:58First of all, Thanks for the help from community. I hope I could be more helpful, more healthy and strong.I saw many questions were answered but the author don't mark correct. Some of the thread were many years ago.I...
Posted on March 09, 2018 at 15:29Is there any HAL_Library to use STMPE811 with STM32F4
Posted on March 09, 2018 at 16:36We are trying to establish and send and receive Project through an ethernet connection .we use Nucleo f429ZI, We have our nucleo with static ip 10.1.1.2 mask 255.255.255.0 gateway 10.1.1.1 using cubemx ,PHY 0,pc is...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.