STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ECDSAsign

Posted on March 22, 2018 at 12:44Hi all,I am currently on a project which leverage the x-cube-cryptolib to send messages cross the network securely. To be specific, I want to use the ECDSA part to sign and verify my messages.  After some exploration...

STM32F4DIS-BB FatFs

Posted on July 14, 2017 at 20:24The original post was too long to process during our migration. Please click on the attachment to read the original post.

dbte by Associate II
  • 7516 Views
  • 21 replies
  • 0 kudos

TIM_ParallelSynchro on stm32f103xx not work

Posted on March 25, 2018 at 18:02I have implemented on stm32f103xx the example TIM_ParallelSynchro, this not work. For stm32f407xx fine work.int main(void){HAL_Init();SystemClock_Config();InitConfigTIM3_Master();InitConfigTIM2_Slave();while (1){}}st...

STM32L011D3 and L6387ED problem

Posted on March 24, 2018 at 12:39Hi,I'm using STM32L011D3 to control L6397ED driver. Everything works fine until supply voltage on L6387ED drops below threshold voltage (typ. 6V). When voltage drop on driver occurs, supply voltage on microcontroller...

Piotr1 by Associate II
  • 2744 Views
  • 6 replies
  • 0 kudos

Best way to configure clock [from scratch project]

Posted on March 24, 2018 at 17:51Hello everyone,I'm starting a blank project and would like to know the best way to configure the clocks (without using CubeMX).The initial project therefore contains the startup file stm32f413xx.s as well as the file...

Jems On by Associate III
  • 3830 Views
  • 7 replies
  • 0 kudos

STM32F0 bxCan Filters

Posted on March 24, 2018 at 22:40 Hello Today i was playing around with the bxCan module in a NUCLEO-F091RC, and trying to understand how the filter works. Afterrading some posts here in the forum i was able to understand the concept of ID ...

Resolved! init nand flash mt39f8g08 in bank3(0X80000000) FAILED?

Posted on March 24, 2018 at 15:27my register set around 0xa0000080 was belowand fmc clock was enablebut i still couldn't reset nand flash and read a error nand id as belowmy reset nand code as below#define READ_ID 0x90 #define NAND_RESET 0xFF #defin...

0690X0000060AE2QAM.png 0690X00000609QNQAY.png 0690X0000060ABTQA2.png 0690X0000060AEMQA2.png

STM32F411 ADC DMA Interrupt, StdPeriphLib

Posted on March 24, 2018 at 19:38 Hi Folks, I am trying to read a potentiometer over one ADC channel of the only available ADC1 peripheral on my STM32F4 board. It works fantastic, when i configure ADC without DMA and when i set only the End of...

tom.abel by Associate II
  • 2138 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.