STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F051K6 Schematics verification

Posted on May 23, 2018 at 16:28Hello Sir,Currently we are working on a industrial project. This is targeted for a monitoring purpose,  which detect by using magnetic flux density sensing.In which we have done a circuit with MCU STM32F051K6, we need ...

jom sabu by Associate
  • 2513 Views
  • 3 replies
  • 0 kudos

5v Tolerant UART on STM32H753

Posted on May 30, 2018 at 17:08Hello,We want to connect a 5v UART device to our STM32H753 MUC through one of the 5v-tolerant UART_RX pins.The MCU IO voltage is 1.8v.The UART is one-directional, from the 5v device to a UART_RX pin, for example PB15.I...

Yan Rosh by Associate II
  • 2390 Views
  • 4 replies
  • 0 kudos

STM32L476 - Elimination of ST Link part

Posted on May 31, 2018 at 09:56Hello, I'm using STM32L476 Discovery board. Using the ST Link (5v), Live Hearing, Record and play back functions are working. But, I'm trying to eliminate the St-Link part from the board, for this purpose i tried givin...

Resolved! Using the ADC MCP3903 via the MCU STM32F072RBT6

Posted on May 30, 2018 at 11:15Hi there, I am new to this community and recently started using STM32 mcus. There is still alot I do not know about this subject so please bear with me. I am trying to get familiar with using these mcus and would there...

STM32H743: What is the purpose of pins FDCANn_TXFD/RXFD

Posted on March 01, 2018 at 14:39We are currently setting up a project using STM32H743 and need to implement CAN / CAN-FD. When activating FDCAN1 or 2 in Cube as Mode 'FD', two additional checkboxes can be activated: Enable_FDCAN_TXFD and Enable_FDC...

GS1 by Senior III
  • 2583 Views
  • 4 replies
  • 0 kudos

F030 UART framing error

Posted on May 31, 2018 at 09:29Hello,I am trying to receive data from https://learn.adafruit.com/adafruit-ultimate-gps?view=all, it should output 9600bd. MCU is STM32F030K6T6. Rx/Tx are crossed as they should be, connected to USART1 (PA2/PA3). I am ...

Real USART2 INT number

Posted on May 30, 2018 at 21:44 USART2 INT number # 26 instead of # I'm building a new project that involve FreRTOS and USART2, when enabling the interruption for the USART2, (Configuration-> USART2 configuration->NVIC Settings) the application s...

ilde by Associate
  • 2601 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.