STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32f4 Timer interrupt

Posted on June 28, 2018 at 13:18 I got program which is requesting measurement results from external device and store them in array. My goal is to generate timer interrupt every 0.5s and process collected results, but it seems like timer interrup...

Resolved! STM32H7 QSPI base address

Posted on June 28, 2018 at 22:54Hi,When memory mapped what is the base address for external QSPI FLASH?I can't find this specified in the data sheet or manual.For the STM32F7 the QSPI base is 0x9000,0000, data sheet table 13.Where is this informatio...

STM32F7 DCMI_DR always zero

Posted on February 10, 2016 at 12:21  The original post was too long to process during our migration. Please click on the attachment to read the original post.

CMSIS-SVD file for STM32F74x is missing interrupts

Posted on June 29, 2018 at 13:27Hello,the CMSIS-SVD files for STM32F74x and STM32F75x are missing interrupt descriptions for the following interrupt numbers:41, 43, 49, 50, 68, 87, 88, 89, 95, 97, 98, 107, 108, 109, 110, 111, 112, 113; thus those in...

UART communication, Not USART case, with STM32F429IGH

Posted on June 29, 2018 at 13:56Hello, I have some trouble to control uart communication with uart port not usart port of STM32F429,I can communicate tx/rx with USART port, even in interrupt mode,but when trying to communicate rx/tx with UART port(U...

STM32F7 and CAN bus implementation

Posted on June 28, 2018 at 20:48Hi,so I am using STM32F769xxx MCU with TI's CAN transreceiver (http://www.ti.com/lit/ds/symlink/sn65hvd232.pdf, see 232 version, the one without low power modes). I have 2 problems that may have something to do with e...

0690X00000604a3QAA.jpg

STM32F334 HRTIM fails randomly

Posted on June 29, 2018 at 10:34Hello.I am using the STM32F334R8T7 in a design of a 3 phase buck converter.I have noticed that sometimes the HRTIM miss the reset event on the PWM (reset means put the output to 0).The frequency is 400kHz (0x2D00 load...

[SOLVED] STM32L031G6U6 only works in debug debug mode

Posted on June 12, 2018 at 09:41Custom PCB using an STM32L031G6U6 (as a slave co-processor to a BLE module, to drive a graphics LCD display). We started with a Nucleo then migrated the project to a custom PCB which implements SWD directly and the pr...

sm23 by Associate II
  • 1133 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.