STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

retriggerable one pulse mode in CubeMX

Posted on February 11, 2018 at 17:47 Hey everyone, Got a little issue that I'm a little confused on. I want to use a one pulse mode to output a pulse of length dependent on the input signal. So essentially, when the trigger goes off, I wan...

0690X00000604MtQAI.jpg 0690X00000604EHQAY.jpg 0690X00000604N8QAI.jpg
con3 by Senior
  • 1657 Views
  • 1 replies
  • 0 kudos

SPI delay between bytes write...

Posted on January 11, 2018 at 13:29Hi,I am using STM32L4 MCU. Facing a problem with SPI communication.MCU clock:48MhzSPI clock enabled as 6MhzUsing a interrupt for SPI write.I am seeing 17us time duration (3us clock + 14ms idle time) between a bytes...

kishore R by Associate II
  • 1215 Views
  • 1 replies
  • 0 kudos

LPTIM Counter in Stop2 Mode

Posted on July 05, 2018 at 10:15Hi, everyone. I'm implementing a shock counter using STM32L476 LPTIM counter & LIS2DH12 click interrupt.I connect LIS2DH12 INT2 pin to LPTIM_IN1 to implement shock counter. ( I expect increment of LPTIM counter when s...

mbedTLS enable DEBUG logs

Posted on December 27, 2017 at 08:15I am using STM32F769I-DISCO. and using STM32Cube_FW_F7_V1.8.0I am testing mbedTLS SSL_Client example.I want to enable mbedTLS DEBUG log in the code.#stm32-f7 #mbedtls

ritesh by Associate II
  • 1114 Views
  • 1 replies
  • 0 kudos

STM32 USB CDC VCP Windows Driver

Posted on April 12, 2018 at 05:49I am developing a product which uses ST USB CDC stack. Windows can list this device as a serial com. I am using ST PID and VID.My question is it seems needs to install ST driver to make this device working. Usually i...

jiangpen by Associate II
  • 1024 Views
  • 1 replies
  • 0 kudos

STM32 CubeMX USB CDC does not transmit

Posted on April 27, 2018 at 23:51 STM32F407VETxBlank CubeMX project template plus USB_DEVICE middleware using CDC classSW4STM32firmware STM32Cube FW_F4 V1.16.0only modified code from generated templates is this (in main.c):  /* USER CODE BEGIN 2 */...

Measured VREFINT value very low

Posted on August 14, 2017 at 02:57The ADC calibration on an STM32F303 is making my head hurt!!I'm using latest HAL library (v1.9.0) and start with calling HAL_ADCEx_Calibration_Start() for each ADC I'm using. I then read the factory calibration fact...

STM32F0 SPI slave mode issue TXRX HAL

Posted on January 13, 2016 at 17:24 Hi, I'm using an STM32F0306 in SPI slave mode *** a sub processor in a project. I used cubeMX to generate the initialization and have added functions in Keil v4 The ST part is in slave mode, 8 bit...

_legacyfs_online_stmicro_images_0690X00000604te.png

LWIP+!DHCP+AutoIP->Custom IP

Posted on February 13, 2018 at 14:27My projects with 32F107 runs DHCP ON works fine on LAN.I want my MCU get custom IP when I connect to PC without DHCP Server.I am using cube and already set Should I use autoIP or insert code when DHCP fail.Do I ha...

STM32F302 CAN interrupt handling

Posted on November 30, 2017 at 09:59Hi,I have some issue setting up CAN for STM32F302 using Keil. As a starting point I used the Keil STM32 CAN Example:http://www.keil.com/download/docs/351.aspEverything seems to work, except the interrupt handling....

paul2 by Senior
  • 1358 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.