STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F767 stuck in hardware reset loop

I can connect with JTAG via SWD and load a simple program but after load the system won't run to main. The chip seems to be stuck in some hardware system reset loop. Attached is an image of the nRST pin. I've gone through AN4661 many times and ca...

0690X000006C4ghQAC.jpg
BGee by Associate II
  • 7728 Views
  • 15 replies
  • 0 kudos

Memory leak check

Hi Team, How can I check memory leak value at different stages of my code & print it as a debug message.

AKulk by Associate
  • 1110 Views
  • 1 replies
  • 0 kudos

Resolved! Using SRAM instead of DTCM on STM32H7?

Hi All,I am developing an application for the STM32H753II using IAR toolchain, STM HAL and Micrium OS-II.Most of the linker script files in the STM32Cube example suite only specify DTCM RAM for data storage (addresses 0x20000000-0x2001FFFF). I have b...

ASmith by Associate II
  • 4682 Views
  • 7 replies
  • 0 kudos

STM32F746IGT - Can't wakeup from Standby

Hi there,I have a custom board with a STM32F746IGT and I'm using the PA2 pin as the wake up source. It's also the sleep source and maybe that is the issue.With all the electronics around it, the system is consuming about 160mA. I can see that it goes...

Resolved! How to initialize STM32L152 UART2 using ST library?

Hi,I'm using the evaluation board STEVAL-IDS001V4M which has a STM32L152 mounted on.I'm having some trouble on the initialization of the UART2 peripheral.I'm using the ST library contained into the STSW-CONNECT009 packet.To initialize the UART2, I'm ...

mikmary by Associate II
  • 2788 Views
  • 4 replies
  • 0 kudos

I2C read issue

Hi,We are using stm32f446zet for a new project . We want to read 3 bytes of data using i2c and the read function is as follows . The 1st two bytes are read correctly but the 3rd byte is always zero . Please help us to solve these issuesint I2C3_ReadS...

adavi.9 by Associate
  • 1020 Views
  • 1 replies
  • 0 kudos

SDIO driver

hi fellows, i'm developing the SD card application for STM32f429 discovery boards. i have the FATFS software with myself. my point i want to develop my own driver for SD card i don't want use HAL driver . i developed the initialization code for SD c...

Ark1 by Associate II
  • 3132 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.