How to lock some of the Flash pages?
Hi.I need to lock some of the flash pages. Is this possible?If it is how can I do this?
Ask questions, find answers, and share insights on STM32 products and their technical features.
Hi.I need to lock some of the flash pages. Is this possible?If it is how can I do this?
This failure happened suddenly with no apparent cause. The board started cycling on/off at a fairly regular frequency (as shown in the attached video). When this happened, LD1, LD2, and LD7 all cycled on/off (LD7 never turns on in normal operation, a...
Posted on December 14, 2015 at 01:07Hi I'm currently developping a RDM responder :) Did somebody of you already took part of a project with RDM ? If so, can I expect some help with my program ? :)Thank you ! #dmx512 #stm32
Hi everyone, i'm trying to read some data from an accelerator and for this purpose using SPI. I'm using NUCLEO-F401RE board. So after enabling SPI, clock pin goes HIGH as i want (CPOL=1) but when i send data CLK stays as HIGH until i disable SPI, mea...
Hello I have two cards, the first is a STM32F746 Discovery and the second is a STM32L475 Discovery.I have to use USB FS to do the firmware updates using the DFU class in USB_Device in CubeMx.I have all tried to update the cards with the DfuSe Demo so...
Is there anyone who worked on RDMDMX with STM32 Controller?
Hi everyone,I'm trying to use LL drivers for STM32F103 series using CubeMX and my problem is that when i try to send a byte LL_USART_TransmitData8(USART1, data) the USART Transmission Complete Flag is never set and no data is transmitted through .I ...
I have been trying to get CAN communication to work using the STM32F4 HAL. I am using the MCP2561 (http://ww1.microchip.com/downloads/en/DeviceDoc/20005167C.pdf) transceiver with the Nucleo board. I have tried using both Normal mode and Loopback mode...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.