STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How do I make I2C work together with DMA without HAL

I've configured I2C and I2C for reading 4 byte from a sensor. But for some reason. I currently don't have the code available here so I'd like to ask if somebody knows of an AN or has managed to receive data using DMA over I2C in master mode.Thanks fo...

CRipc by Associate
  • 750 Views
  • 0 replies
  • 0 kudos

STM32F103VET6 flash corruption

Hi,I have a board with STM32F103VET6 mcu. Sometimes when power on at startup, my mcu sometimes does not start as it should start, and it only start to work when the software is reinstalled.When the problem occured, I have checked the flash data from ...

0690X000006CNckQAG.png
er3481 by Senior
  • 1091 Views
  • 2 replies
  • 0 kudos

HSI calibration step on STM32F7 and STM32F0.

When I calibrate the HSI frequency of an STM32F7 writing to HSITRIM in RCC_CR register, which is the calibration step? I mean, how much the frequency of HSI change if increasing or decreasing HSITRIM in 1?Doing the same with an STM32F0, ref. manual s...

IHugu by Associate
  • 842 Views
  • 0 replies
  • 0 kudos

i cannot use X-CUBE-MEMS1

https://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-mems1.htmli downloaded this software.i also used the gui program. but i have to read under 0.01g so gui...

khyun.8 by Associate
  • 804 Views
  • 0 replies
  • 0 kudos

software reset problem if reset from a task

Posted on January 21, 2014 at 14:29I use NVIC_SystemReset() in order to reset the system.  I am using STM32F103 in my application and RTX rtos. The problem is that if  called NVIC_SystemReset() before the RTOS started, the software reset worked. If ...

huiyan by Associate
  • 3998 Views
  • 5 replies
  • 1 kudos

How to calibrate the RTC accuracy?

I'm using the STM32F767ZI MCU and with its RTC function. But my quartz crystal is not accurate. According to the document of the MCU, the accuracy can be calibrated (it said in page 35/255: Digital calibration circuit with 0.95 ppm resolution, to com...

HFeng.2 by Associate
  • 842 Views
  • 0 replies
  • 1 kudos

How to check the SPL version?

I found a version macro in the library but it seems to be wrong. Please see attachment. What should I do to check the SPL version in the code?

TMark.8 by Associate II
  • 1173 Views
  • 0 replies
  • 0 kudos

MB1314B AMOLED board schematic

Hello, We are developing a watch-like wearable device with LCD. STM32L4R-Discovery board is a nice reference design for STM32L4R+AMOLED development. It would be also nice to have a schematic for the adapter board MB1314B, which the AMOLED is attached...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.