STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-F303RE ADC interrupt issue?

Hello everyone,could someone please help with the following, I am trying to use ADC with interrupts. Doing the same thing with STM32F103C8T6 it works without issues, but using nucleo board it doesn't.Could someone please have a glance on the code ? (...

Resolved! Issue with PLL of the STM32F302

Hello, we're using the microcontroller STM32F302C8 and we have a problem with the PLL.The problem is when we enables the PLL the microcontroller is reset. We have made several tests using HSI and HSE, but always the same result, a reset after to enab...

GYacc by Associate II
  • 3143 Views
  • 4 replies
  • 0 kudos

STM32F746 Discovery default screen reset

I am new to Electronics and recently bought STM32F746 Discovery Board and connected to to my laptop using USB cable to STLink connector pin. Main screen light up showing programs pre save in it. and uploaded run LED blink code and then screen went of...

MMalv by Associate
  • 1400 Views
  • 1 replies
  • 1 kudos

Is the 4mA increase in current consumption expected when we just enable the wide bus operation in uSD card via SDMMC interface in STM32 MCU?

In a product which requires power consumption to be minimum as possible, we are employing a STM32L496 as MCU. In recent days, we were trying to bring down the power consumption of the overall device. We observed that immediately after enabling the wi...

HP.15 by Associate II
  • 2073 Views
  • 4 replies
  • 0 kudos

Vbat measurement way off (0.15V)

I use the Vbat pin to measure a lithium battery (3.6V) at a STM32L471 (Vcc=1.8V Vdda=3V).However my measurements are off by ~0.15V even though I confirmed the physical signals.Do I have to calibrate the ADC somehow for this to work properly?Expected ...

michael.m by Associate II
  • 1570 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F429ZIT6 doesn't start without debugging session

Hey Guys,I have designed a custom board with the STM32F429ZIT6 which I programm with the STLink debugger together with TrueStudio. So far everything seems to work except that when I don't use a debugging session I have to manually make a reset on NRS...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.