STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use program outside the main while function

Hi there,I am transmitting and receiving data via uart like an pl2303 bridge via USB FS. How can i manage the transmitting and receiving process outside the while so that i not block the mcu?int main(void) { USB_CDC_STATUS_t check_usb; uint16_t r...

arduo by Senior
  • 1475 Views
  • 2 replies
  • 1 kudos

STM32F1 DMA+GPIO Issue?

I need to transfer parallel data via GPIO and DMA. The microprocessor I use is STM32F103C8I need to transfer some memory data to GPIO quickly. I've written an init code using STM32F103 and the HAL library. But DMA doesn't work. At the end of the proc...

FreeRTOS USB Host example

I need a STM32F411 DISCO USB Host example using FreeRTOS.My project is based on STM32F401. I don't have target hardware yet & have survived with a NUCLEO 401 and linking wire. That won't be good enough for USB.Nearest is a STM32F411 DISCO but my rush...

PRobe by Associate II
  • 856 Views
  • 0 replies
  • 0 kudos

Can't connect to COM Port

Hi,I implemented a composite device program for my mcu (STM32F407IG) .Everything is working fine and the mcu get recognized as cdc+msc.Somehow it won't connect to the vcp when i am using a terminal program like HTerm to send data to vcp.Anyone have e...

arduo by Senior
  • 826 Views
  • 0 replies
  • 1 kudos

USB Composite Device Driver

Posted on September 19, 2016 at 08:59Hi all, for my project I developed an USB composite device (MSC + CDC) based on an STM32F2.Since ST doesn't provide an example of a composite device based on the HAL, it wasn't so easy to have my device working, ...

Lori B. by Associate III
  • 4577 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.