STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Enable upload to homemade STM32F405 evaluation board

Disclaimer - my skill level is pretty low but I am very keen to learn :D I made this homemade STM32F405 evaluation board and using STM32 Cube-MX, Keil uVision 5 and a ST-Link programmer was able to upload a basic blink code example. However I am want...

pedro1 by Associate II
  • 4362 Views
  • 9 replies
  • 0 kudos

ili9341 and pins

Hello guys,I would like to drive ili9341 using that library --> https://github.com/martnak/STM32-ILI9341and I faced somthings that I didn't know about pins.My device is this --> https://tr.aliexpress.com/item/3-2-inch-320x240-320-240-TFT-LCD-Module-...

Zek_De by Senior
  • 1562 Views
  • 1 replies
  • 0 kudos

Running code in RAM on STM32H7

Hi,I have to to run my code in RAM on STM32H7 and debug it.I put my code in RAM_D1 (start address = 0x24000004) changing the linker file in this way: /* The program code and other data goes into FLASH */ _sl_my_Code = LOADADDR(.my_Code); /* pnt to th...

ADion by Associate
  • 1828 Views
  • 2 replies
  • 0 kudos

Nucleo F303RE USB Serial Comm HAL example code?

Hello,I suspect there's example code for reading and writing serial data through the USB comm port (ST-link cable) on the Nucleo boards using the HAL libraries. Can anyone point me to one? I've seen the printf() example which is half way there. Th...

How to get started with bluetooth?

Hi, I've had an STM32F411 development board for sometime and have done hobby projects with practically every peripheral on the board (audio output, mic, accelerometer, gyroscope, etc) programming both with and without the HAL. I'm now interested in ...

Resolved! STM32F0: updating RTC calendar after wake-up from standby fails.

Hi all,I'm faced with a strange issue: updating the RTC calendar does not seem to be possible after a wake-up from standby mode.I have a piece of code that updates the RTC calendar (date and time are uint32_t):// rtc disable write protection RTC->...

APann by Associate
  • 1644 Views
  • 1 replies
  • 0 kudos

Resolved! Do RAM may have old data after energized

Hi everyone ,We are using our custom bootloader firmware to update our main firmware.To do that we set a flag at a specific location at RAM and reset the MCU.The flag size is 1 byte.At the bootloader firmware read the data from RAM and if this data m...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.