STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F303RE Nucleo Board HAL_USART_Receive_IT problem

As the title suggests, im having a problem using HAL to make some USART echo.I tried the same approch on a nucleo-f031 and its working wonderfully.I can print the whole hyperterminal string, but i cant reach the receive interrupt. Even if i set the R...

AWeis by Associate
  • 765 Views
  • 0 replies
  • 0 kudos

Resolved! When does STM32G4 arrive?

The official release of STM32G4 was scheduled for the 20th week of 2019, but now we are in the 21st week and there is still nothing. Any problems?Andrea

Resolved! Low Power Timer Wake Up from Stop2 (stuck in interrupt)

I am using a STM32L476. I am using the counter mode on the low power timer to generate an interrupt after a given period. When I am in run mode, this interrupt works just fine. However, when I use the interrupt to try and wake the MCU from Stop2, I g...

Resolved! How to calculate CRC for large file in STM32F030RC

Posted on February 03, 2018 at 07:45I want to calculate CRC for large file, the large file have been added the CRC value in the end of the whole .bin file(Get this CRC data via IAR tool). I read the file and calculate CRC of it in part(HAL_CRC_Calcu...

Hal stm32f103 and dds problem

i have problem with data ud and clk signals out to dds.its not a steady stream to dds.in the oscilloscope the data,clk ud signals are not stable.the signal are moving and jumping around so the dds of course gives weird and wrong freq.i tried intern...

Molof by Associate II
  • 2083 Views
  • 5 replies
  • 0 kudos

Interrupt gets executed but the CPU stays in WFI

stm32f407i code in RTEMS, system sleep function will call __wfi , i can not wake up from sleep by pressing keyrtems_isr EINT95_handler(rtems_vector_number vector) { if(EXIT_PR & 0x200) { printk("exit 9 hap\n"); int pin = STM...

IWDG trapping

Hello,I activated the IWDG on a STM32L431 device and a watchdog occurs. How could I trap it to find the issue?This watchdog resets the device so I do not know how to find the stack values when this watchdog occurred.Is there a way to send this IRQ to...

Mich1 by Associate III
  • 1856 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F407 I2C1 EV and ER Interrupt Problem

Hello Everyone,I have dealing with STM32F407 I2C peripheral in order to implement Non-blocking communication.I have made many trials but I2C1 event and error interrupts never occur. I checked the SB bits during the debug mode it becomes 1,the other r...

hakand by Associate
  • 1482 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.