STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Executing independently compiled code in RAM.

I have a device that must execute precompiled functions which are copied to a place in RAM. Function calling:PLC_main = (pFunc_main) 0x30000001; PLC_main();Compied function: PLC_1 0x30000000: 4811 .H LDR r0,[pc,#68] ; ...

VNilo by Associate
  • 1401 Views
  • 2 replies
  • 0 kudos

Temperature of the internal temperature sensor

Using STM32F0308C on a custom board. When I read the temperature sensor I am getting 1765 and the TS_CAL value is 1778.Supply voltage is 3.3V, VREF_INT is 1524 and I am reading 1525 on the internal reference. So I assume I must apply a 1524/1525 corr...

ECost by Associate II
  • 1282 Views
  • 1 replies
  • 0 kudos

I am using STM32F030c8t6 in my device which is battery operated. I want to monitor a standard 3.7V Lipo battery voltage so I used a voltage divider at the battery and divider output is set to 3.3V which goes to ADC pin of Controller.

1. Is it ok to set 3.3V as a divider output which goes to ADC pin?2. The external voltage at VDDA pin (We have given the same VDD as VDDA) show some fluctuations while ADC monitoring so can you suggest the best possible way to monitor battery voltage...

HRawa by Associate II
  • 967 Views
  • 0 replies
  • 1 kudos

Mismatch datasheet reset value and reality

Dear community,I am using the STM32F103C8T6 32 bit ARM Cortex M3 microcontroller.In Section 9.2.1 in the reference manual (GPIOx Control Register Low) it says that the reset value is 0x4444 4444 (which means all pins are floating inputs).However, whe...

Xhendos by Associate
  • 801 Views
  • 0 replies
  • 0 kudos

Timers frequency divided by 2

Hello everybody!I try to configure TIM2 to interrupt in the range of 100Hz ... 1kHz. Strangely, the actual frequency I set is divided by 2: if I configure the timer to run at 1000Hz, it will run at 500HzTIM2 configuration:void System::InitTimers() ...

jean by Senior
  • 1927 Views
  • 8 replies
  • 0 kudos

Minimum ADC Sample Times

Looking at the datasheet for STM32F20xxx ADC; if I run the ADC at 30MHz and use the minimum sample time of 3 (100ns), the input sample capacitor will not be fully charged even with zero source resistance. The input spec is 6K and 4pF, if you take th...

JKing.3 by Associate II
  • 717 Views
  • 0 replies
  • 0 kudos

Timer Configuration causes Flash Error

I've got a real strange error, and I really don't understand it. I'm using a STM32F407VET6 Microcontroller. I also use CubeMX to generate the configurations. But especially with the Timers, it's not possible to set every setting I need with Cube, so ...

user 143 by Associate III
  • 3003 Views
  • 4 replies
  • 0 kudos

How to fix the Files Upload Problem

I'm a tiro of ST-LINK/V2 and STM32 tools.Recently, when I upload a file via ST-LINK/V2 to my STM32 tools (OpenIMUZA300), the upload prosess was failed.The warning messages are:no flash bank found for address 0x10020000no flash bank found for address ...

0690X000009YRMSQA4.jpg 0690X000009YRMcQAO.png 0690X000009YRMhQAO.jpg 0690X000009YRMmQAO.jpg
ZZhao.12 by Associate
  • 834 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.