STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How do I save application data on my MCU in NVM?

I'm using the STMF1 series and the HAL drivers. I already use a boot-loader to write into application space. However, now the the application to take some input data and save it permanently to a non-volatile-memory space. I assume I can use the HAL_...

DJC by Senior
  • 3518 Views
  • 6 replies
  • 1 kudos

Resolved! SPI Receive problem

Posted on June 27, 2017 at 06:45Hi all,I am trying to read a four bytes register from TDC-GP30 ultrasonic flow converter using HAL_SPI_Receive function. Below is the code that I am using for reading the register contents:/***************************...

Resolved! ADC with LCD “Hello world�?

Hello ST Community,in the folder STM32Cube/Repositery/STM32Cube_FW_F4_V1.24.1/Projects/STM32F413H-Discovery/Applications/STemWin/STemWin_HelloWorld.I debug it into the card, it works but now i wanna use the ADC to convert some analog data and display...

idrissmc by Associate III
  • 1448 Views
  • 3 replies
  • 0 kudos

Digital Image Processing with STM32 ?

Dear Members or ST Employee,I've been looking for inspiration from STM32 board for digital image/signal processing,Any boards that can be used for image processing straight away from development board?because I need RAM for it, and the internal RAM w...

STM32L4 VRefint dependency on temperature

VRefint is between 1.18 and 1.22V depending on temperature. As in our hardware we have termometer available i would like to know more precisely what Vrefint voltage actually is.What are exactly the relation between temperature and Vrefint voltage?equ...

WPuch by Associate II
  • 716 Views
  • 0 replies
  • 0 kudos

Implementation of filesystem

Hi i am trying to implement Littlefs filesystem on STM32L151 MCU which is interfaced with external Flash memory using SPI.is it already implemented on any one of the STM32 board? if yes-i need to know what are the key features to be carried out to im...

Rekha.k by Associate II
  • 3441 Views
  • 4 replies
  • 1 kudos

AHB and APB

Hi ST Community,I’d like to know why sometimes we use GPIO with AHB and sometimes with APB ?

idrissmc by Associate III
  • 3355 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.