STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bootloader and main firmware clock config

Hi ST Community,I have a device built on the STM32F407, with my bootloader.If the bootloader runs at 168 MHz, and the main firmware runs at 72 MHz, everything works fine.If SystemClock_Config of the bootloader have same settings (dividers and multipl...

ALavr.10 by Associate
  • 794 Views
  • 0 replies
  • 0 kudos

Resolved! Nucleo-L011K4 USART examples not working?

Hi,I got a brand new Nucleo-L011K4 and was very interested in testing the examples I got from ST, but when I download the USART examples on my board the receive part of them does not work. Is there any flag I need to set/clear that the examples are m...

The QSPI Indirect read mode doesn't work

All QSPI Receive functions(receive, receive_it, receive_dma) collapse when fmode is loaded with indirect read mode(01) in case ADMODE, ABMODE and IMODE fields are zero. On STM32H743ZIT Dev board

LKauf by Associate
  • 764 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F7 High Power Consumption in Standby

All, Unfortunately I don't see many useful answers to high standby power consumption on these forums. Hopefully someone has gained insight since previous questions have been asked, or my specific situation is has an alternative solution that didn't a...

ZThat by Senior
  • 3237 Views
  • 5 replies
  • 0 kudos

STM32L476 FatFs. cannot mount sd card (F_mount) - Help!

Hi,Another one for you.I am having problems with the FatFs library, specifically I cannot mount the SD card. I am using the HAL libraries and have generated the configuration using STMCubeMX. I cannot get this to work on either my own hardware of t...

Clarify maximum CPU frequency

Hello,I'm confused about the capability of STM32H753 to operate at a CPU frequency of 480MHz.The datasheet mentions that 480MHz is the max CPU clock frequency under VOS0, and the reference manual describes how to activate voltage scaling to VOS0.Howe...

Gpeti by Senior II
  • 3226 Views
  • 8 replies
  • 0 kudos

STM32L071KZ I2C Slave mode Code

Hello Everyone,I am working on STM32L071KZ for my next product.I have reached a level where I have to make STM32L071KZ I2C1 work in Slave mode.For making this controller I have got some sample code on the internet and tried but I am not able to this ...

Vijay1 by Associate II
  • 914 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.