STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IAP for STM32L011

Hello,Is it possible to have in-application-programming (IAP) on STM32L011F4? I can see the IAP example listed under STM32L073Z-EVAL but I am not able to build for STM32L011K4. Just to give an example: macro OB_BOOT_BANK1 is defined only when setting...

RPrun by Associate
  • 1144 Views
  • 1 replies
  • 0 kudos

Resolved! ADC trigger with timer not working

Hello,I have a small issue with my code. I am using the NUCLEO-F746ZG board and I want to do a small program that reads an ADC triggered by a timer.Here are my init routines (generated by CubeMX):ADC: hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler ...

Stabilo by Associate III
  • 2877 Views
  • 1 replies
  • 0 kudos

Does WriteProtection require POR with JTAG/SWD connected?

I'm enabling write protection on the flash on my STM32l451RE, but as soon as the OB Launch is called while the debugger is connected through JTAG/SWED, when the device restarts it seems like it enters an unknown state, just as I would have expected f...

FDane by Associate II
  • 793 Views
  • 0 replies
  • 0 kudos

Resolved! Look for CAN example for STM32F4

안녕하세요. stm32446re 로 공부하고있는 학�?입니다.몇가지 질문사항�?� 있어서 여쭤봅니다.1. can통신�?� 하고�? 하는�?�, can 2.0b를 �?�용한 예제를 혹시 받아 볼 수 있�?�까요?2. f446re 와 f429zi를 �?�용하여 can 통신후 모터를 �?�리고�? 하는�?�, 모터 예제�?� 받�?� 수 있�?�까요?  미리 �?사�?�사 드립니다 ^^

KBumS by Associate II
  • 2977 Views
  • 5 replies
  • 0 kudos

Missing Datasheet for ST33G1M2A.

I need datasheet for ST33G1M2A part, but only databrief document was coming in front. Databrief details are highly insufficient for me. Please support and help me getting this datasheet. Complete Part#: ST33G1M2A020FAA5Thanks in advance.

PS.141 by Associate II
  • 2024 Views
  • 3 replies
  • 0 kudos

STM32L432KC Core Bug ?

Dear All,Do you find any VSSA (VRef-) pinout on the STM32L432 32QFN ?The Analog Input never stable !! when PA_1 NC, PA_0 result:0V = 7FFH3.3v = FFFHwhen PA_1 to GND, PA_0 result:0V = 0H3.3v = FFFHwhen PA_1 to 3.3V, PA_0 become floating....I can not...

JLiao by Associate II
  • 827 Views
  • 0 replies
  • 0 kudos

How to write programs for STM32

I often write here that I don't use Cube/CubeMX. This sometimes rises questions, e.g. one forum member asked me off-forum:> What would be the best way to program STM32 MCUs ?> Don't you use the cubemx generated code ?> Have you some sort of good guid...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.