STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G0 - Determining Vref

Hi, using STM32G071 Nucleo Board.Set Vref to internal 2.500 Volt.Set jumpers accordingly (SB28 ope´n, SB21 close) and measure 2.5001 at pin AVDD (CN5.8) on Nucleo Board. So far, so good.Now try to determine AdcVref in software by reading ADC_CH_VREF ...

JuM by Senior
  • 2534 Views
  • 3 replies
  • 0 kudos

Handling filters for CAN1&CAN2 and FIFO0 & FIFO1

Hi everybody,I'm using an STM32F469BI and I'm trying to receive on both Can1 and Can2, and handle messages on both FIFOs. For example, my board can be commanded to wait for messages on CAN1 FIFO0 and CAN2 FIFO0 or CAN1 FIFO0 and CAN2 FIFO1,..So i'm a...

Steven.D by Associate II
  • 1474 Views
  • 0 replies
  • 0 kudos

Can't write to CM4 core

I have an stm32h745zit6 on my own board, where I can write correctly to the CM7 section (0x0800 0000 to 0x080F FFFF range) but not to the CM4 section (0x0810 0000 to 0x081E FFFF range), I also can't do a full erase of the chip, and it will give me an...

Skippy by Associate II
  • 2535 Views
  • 5 replies
  • 0 kudos

Can NAND flash be used with STM32L475VGT6

I want to used NAND Flash with QSPI interface in STM32L475VGT6. Its not clear in the datasheet if NAND can be used on one page NAND driver shows up on block diagram and another one under the revisions of the part it says NAND has been removed.Can you...

BBV by Associate II
  • 1417 Views
  • 2 replies
  • 0 kudos

STM32 Confusing users with description of Vref and VDDA

Hi,in my opinion there is some confusion in description of VREFINT_CAL and VREFINT_DATA to determine VDDA.My opinion: One determines VREF, not VDDA. One does not need to know VDDA in respect to measured values by ADC. One must know VREF (no matter if...

JuM by Senior
  • 2004 Views
  • 3 replies
  • 0 kudos

ADC Sampling Without Any Delay For 1 Minutes

I need to save adc data for 1 minutes. I am using ADC interrupt for 2651 sample per second. I have 2 buffer on adc interrupt. In main, in the while section if flag is 1 i am writing adc1 buffer values to sd card with dma. If flag is 2 i am writing ad...

D.K. by Associate II
  • 607 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.