Ask questions, find answers, and share insights on STM32 products and their technical features.
Hello community,I am trying to use the capture feature on the comparator. I want to use it in low power mode. Right now I have something similar to the logic below:enable capture; //just to say that the capture interrupt is enabled here while(!capt...
Good afternoon,I have a stm32l432kc microcontroller on a custom board with two voltage supplies:1) A LiPo battery where I use a regulator to supply 3.3v to power everything and 2) A coin cell battery to only provide power to the RTC within the micro....
Hi, I have configured two 16-bit general purpose timers in master slave mode and made 32 bit timer to get the time base ranging from micro seconds to minutes. I want to configure two 16-bit LP timers to wake up the system after for specified time ran...
Hi,I am using STM32l072CZYx. I am generating the PWM using timer 3 channel 2. But PWM is getting trigger by SPI, PWM is resetting for some time. When I disabled the SPI, I am getting exact PWM. What will be the reason?What can be done to avoid such...
I have the STMf32f469 board , when I try to send a demo to the board it says that I do not have the St link utility ? Shouldnt I have got that with the StmCube install ? Or do I need to download that specifically ?EDIT> Worked with ST link. Although ...
Hello!I have a quite specific question about STM32L4-MCUs. For a project, I would like to use code Readout Protection (RDP), but I have to be able to mass-erase the chip and manually upload a new image. So only RDP level 1 is an option. But with RDP,...
What is the schedule for the STM32H745BIT6 Processor. Meanwhile it is in active state on the ST homepage (But not in CubeMX).Is there an estimation when it will be available for distrubutors? Is there a possibillity to get ~5 samples of this chip dir...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.