STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am designing STM32F429 to access NOR Flash S29GL01GS. Refer to RM0090 reference manual, I am using FSMC to perform asynchronous read. What is the correct value for NOR_Timing.DataSetupTime? How do I calculate it?

Below is the ST sample code. /* NOR device configuration */ NOR_Timing.AddressSetupTime = 1; NOR_Timing.AddressHoldTime = 1; NOR_Timing.DataSetupTime = 6; NOR_Timing.BusTurnAroundDuration = 0; NOR_Timing.CLKDivision = 2; NOR_Timing.DataLatency = 2; N...

cye.15 by Associate
  • 831 Views
  • 1 replies
  • 0 kudos

STM32 with UART protocol sensors (URM07 ultrasonic sensors)

Question: What function could be used/ written to receive the data (URM07)?Currently, integrating an URM07 ultrasonic sensor on STM32f1xx, according to the datasheet the transmission, have tried the function on UART (HAL_UART_RxCpltCallback) to recei...

ELim by Associate II
  • 3549 Views
  • 5 replies
  • 0 kudos

Stuck in UART_WaitOnFlagUntilTimeout

Hi,I'm trying to transmit/receive data by uart. I have a state machine that is processing incoming bytes periodically, so I use a ringbuffer and write every received byte into this buffer.void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart){  if (...

KR51K by Associate III
  • 1209 Views
  • 0 replies
  • 1 kudos

STM32F7 QSPI Flash External Flash Loader

Hello to everyone. I am currently developing a project using STM32F750N8 and W25Q128. As you can guess, the project has an LCD. So the project is too big to fit into the internal memory. That's why I need an external memory integrated programming. I ...

Problem with B-L475E-IOT01A connection to the PC.

Hi everyone, first of all, sorry for my english, and I don't know if i should post this here, so i'm sorry if not.I have a problem when i connect the B-L475E-IOT01A board to the pc. It shows me a error message: "error, not recogniced device connected...

STM32L4R9-Discovery and external PSRAM

Hello,I am currently working with a STM32L4R9-Discovery board with STemWin using demonstration project.I want to use the external PSRAM as a memory for the LCD GFXMMU framebufferfrom LCDConf.c :#if defined ( __ICCARM__ ) #pragma location="FrameBuffer...

STrop by Associate II
  • 1650 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.