STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DAC with DMA

Hi,I'm using DAC with DMA to implement a shape generator on STM32F746.So i'm creating a buffer filled with the datas of the shape concerned that i transmit to the DMA with HAL_DAC_Start_DMA() function.While most of the time everything is ok and the s...

JFric by Associate II
  • 1202 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F207VE UART Routing mistake

Hi,I have design a custom board with the STM32F207VE. But I made a mistake in routing the UART TX as RX and UART RX as TX. Is there a way to change the STM32 UART TX port to an RX through the software?

JTan by Associate II
  • 3877 Views
  • 9 replies
  • 0 kudos

STM32G431KB BOOT MODE

The manual writes: At startup, a BOOT0 pin (or nBOOT0 option bit) and an nBOOT1 option bit are used to select one of three boot options:But I did not find nBOOT1 in Pin definition. I don't know how to configure the pins of BOOT mode.

km naxin by Associate II
  • 1168 Views
  • 1 replies
  • 0 kudos

Resolved! LPUART configuration in STM32L4R5ZI board

Hi,I am using STM32l4 nucleo-144 board to create an example application for LPUART1 communication.Part number - STM32L4R5ZII have configured the GPIO and required clocks. But still not able to do a successful transaction. /* Enable Power Clock */ ...

SP.3 by Associate II
  • 4204 Views
  • 6 replies
  • 0 kudos

CanBus Simple Code Not Working

I made a simple connection like in the figure. The processor's Tx pin is connected to the Rx pin. When I look through the oscilloscope, I can see the data flowing.When I debug code :It goes to the error code in the picture during tx.Code:CAN_FilterTy...

0690X00000AqN24QAF.png 0690X00000AqMZRQA3.png 0690X00000AqMxsQAF.png 0690X00000AqMxxQAF.png

stm32f7 file operations on 8GB eMMC

Hi,we have custom board based on stm32f7 and 8gb emmc is mounted on the board.As i see in other posts,we are also seeing CID,CSD values which results in 1gb capacity(not 8gb capacity).At the moment we don't want to execute EXTCSD and recalculate act...

Tp by Associate II
  • 4782 Views
  • 5 replies
  • 0 kudos

Can't read measurement registers from MPU6050 via i2c

I am trying to read the measurement registers from MPU6050 via i2c, the MCU was able to detect the MPU6050, but i am not able to read the measurement registers, i am using the Hal i2c drivers and i have pasted my code ? int main(void){  /* USER CODE ...

ADC with DMA reads random zeros

Hey there, I'm using a STM32H742 Eval Boards to read analog data with the ADC with DMA. I want to do multiple measuremts very rapidly.In the first measurment the ADC reads a couple Zeros (see plot, note: plote is bit older and has multiple measurment...

0690X00000AqLOIQA3.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.