STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F051R8T6 GPIOC Alternate Function / TIM3_CH3 on PC8

Hello,I have tried to set the brightness of the blue LED on the STM32F0DISCOVERY via TIM3, not using the HAL or LL driver, but writing the appropriate registers directly, with no sucess.The peripheral register view shows that any write to GPIOC_AFRH ...

UART not working correct when using with CANBUS

Hi,I have generated the code using CUBEMX.In my code i'm trying to send data over CAN and USART .CAN is working as i have tested with my analyser but over USART sending some junk data.is there any possibility that CANBUS and USART gets conflicted.i'm...

0690X00000AqaTXQAZ.png
VPras by Associate II
  • 2010 Views
  • 4 replies
  • 0 kudos

In-application programming over CAN BUS

So we are checking a solution based on STM32F4 family (in this case) ARM MCU.We have found an Application Note (AN) for the In-Apllication Programming (IAP) for Ethernet, UART and even USB, but nothing for CAN Bus. In the AN there is a statment that ...

FGasp.264 by Associate II
  • 3108 Views
  • 4 replies
  • 0 kudos

CCMR1/CCMR2 register in STM32F407 for input Capture mode.

Hi,I want to use input capture mode to detect event at every edge (STM32F407 Discovery board).I have toggled the LED (Connected to PD12) using Timer4 Channel (TIM4_CH1) Output compare mode. It's working. The output of LED is given to PD13 to count th...

Kumar B by Associate II
  • 2753 Views
  • 4 replies
  • 0 kudos

As5048a read encoder spi mode

hi I should read the value of the angle of the encoder as5048a via spi, the register has address 0x3fff, a 14-bit register, I tried in several but I failed, can you help me? I use a f401 !! thanks

SDall by Associate II
  • 4474 Views
  • 7 replies
  • 0 kudos

Resolved! L031K6's internal reference voltage is 1.1v?

hello, I am using L031K6 nucleo-32 board.for using low-power-comparator, I want to use VREF for input.before using, I did measure the internal reference Voltage by ADC.L031K6's VREF have internal connection with own ADC VREF channel,so without hardwa...

DU2 by Associate II
  • 1000 Views
  • 1 replies
  • 0 kudos

H7 series peripheral performance in VOS2 and 3

The datasheets for the interface characteristics of each peripheral state "VOS level set to VOS1" which is the 400MHz option. But no information is given on if any of the peripherals derate if you use the slower speed and power VOS options. Would ...

MikeDB by Lead
  • 2750 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.