Ask questions, find answers, and share insights on STM32 products and their technical features.
I am using STM32F105 (25Mhz crystal freq)with atmega16. cycle of data sending:1.STM32 to ATMEGA16.2. ATMEGA16 to STM32.first cycle is working fine but in second cycle atmega send data perfectly but stm32 not receive receive continue data.
Hello, i am going through the the technical reference manual of STM32L4R5 and i am bit confused about the Flash Protection feature, specifically write protection feature.my product requirement is to avoid the modification of my executable ( bootloade...
stm32h743iiWhen we set the OSPEEDRy[1:0] = 11 we have glitch spike (undershoot) on clock and data. it was improved when we set OSPEEDRy[1:0] = 01.In datasheet SPI interface characteristics page 307 saidOutput speed is set to OSPEEDRy[1:0] = 11.
I have purchased STM32H750B-DK. I am using system workbench for stm32 as IDE. Now i downloaded STM32CubeH7 library and trying to download GPIO_IO_Toggle example program into this board but getting the error as below:17:31:42 **** Programming project ...
What is it that I've been missing...I set a timer to trig 7-channel ADC with DMA. The DMA is set to make 7 16-bit to 16-bit transfers circularly. It seemed to work fine, but some data started to corrupt. So I made the 7x16-bit buffer 4-fold (28 16-bi...
Hi,I'm trying to configure SDMMC module using DMA since I'm using FREERTOS. But in STM32CUBEMX, there is no option to configure DMA settings under FATfs.So, I'm trying to setup the DMA configuration through code. I can see that there is no definition...
Hi,I have two B-L475E-IOT01A boards and I am testing the SubGHz P2P application available in the STM32CubeL4 package. Whenever I press the User Button on one board the led LD1 on the other board blinks, and as the ACK command is received the led LD1 ...
I want to calculate the measurement accuracy.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.