STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The accurate of integrated RTC in STM32F103C8T6

Hello everybody, I want to design an application with RTC, I was very impressive with the accurate of DS3231 with small deviation for long time working.But the chip DS3231 is quite large meanwhile RTC is already integrated in STM32 also. I just want ...

using the following J-LINK FLASH tool . I need to do some additional configuration for STM32F217VG in the J-FLASH tool . Does anyone has the settings

I want to read 1 MB flash contents from STM32F217VG starting at address 0x0800_0000 to 0x0810_0000using the following J-LINK FLASH tool . I need to do some additional configuration for STM32F217VG in the J-FLASH tool . Does anyone has the settings a...

0690X00000AtD59QAF.png 0690X00000AtD54QAF.png 0690X00000AtD4zQAF.png 0690X00000AtD4fQAF.png

IAP does not jump to the desired address.

Hi, I am using STM32H753VI on my own board. I was trying to programme the chip using SDCard through IAP. the program works perfectly till it erase bank1(from 0x08020000 to end of sector7 of bank1) and whole bank2.then copies the bin file to flash. ev...

dv.13 by Associate II
  • 2404 Views
  • 5 replies
  • 0 kudos

OTA for STM32F070CB,STM32F070C6

OTA is possible with esp32 wifi module ...? for these microcontrollers if not possible which series microcontrollers have that facility. If possible can guide me plzz...?

AVenk by Associate
  • 660 Views
  • 0 replies
  • 0 kudos

touch sensing calibration

HiI'm working on touch sensing feature of stm32f051,,but I have a big problem that every board that I assembled has different thresholds for its sensors(the component are the same) and I can't have a unique code and each time I have to change thresho...

STM32 RTC Alarm behavior

I am currently making a device running the RTC calendar. The MCU will be in stop mode for the most of the time. It will wake up in the certain date and time. Is it possible to configure the STM32 to wake up once a month by setting the alarm day and t...

Leo Tai by Associate II
  • 851 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.