STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to establish LIN communication between two STM32F MCUs?

I would like to implement LIN communication between two STM32F series MCUs.But so far, I did not find any example code for LIN implementation using STM32F MCU.Can you please share sample code of LIN communication using STM32F which includesInitializa...

SPate.14 by Associate
  • 807 Views
  • 0 replies
  • 0 kudos

Stm32 footprints

Hi ! Do ST released footprints library of chips for example for eagle?​Im trying to make new library device for schematic and pcb. But it would be superb if I could just download it.​Stm32f103c8 lqfp48

oeliks by Senior
  • 870 Views
  • 0 replies
  • 0 kudos

Resolved! I'm specifically using the discovery kit for the STM32F746G - Disco board. I've used STM32CubeMX to generate the configuration with no mods and then the code for atollics Truestudio, keep getting interrupts from TIM6

i can see both in the tool and the source code that the TIM6 timer is not configured. It is in fact the TIM6_DAC_IRQHandler() I keep ending up in.Now it's easy enough to just force it to be disabled but I'm trying to figure out how to disable it in t...

jdowdster by Associate II
  • 1726 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F745 suddenly is extremely slow - have I bricked it?

Hi,I've been working on programming my STM32F745 for some months now, step by step playing with the different peripherals. So far so good. I've been also doing step-by-step debugging with OpenOcd and STLink V2.Today things started to look a bit weird...

CGalv by Associate III
  • 1681 Views
  • 3 replies
  • 0 kudos

STM32L452 QSPI Errors

I'm using the STM32L4 Nucleo board with a N25Q256 SPI Flash attached. I can successfully read and write from the spiflash using the QSPI peripheral + HAL layer in standard SPI mode. However when switching to Quad mode, every so often during a longer ...

0690X00000BvwAgQAJ.png 0690X00000BvwAqQAJ.png
dan0 by Associate II
  • 726 Views
  • 0 replies
  • 1 kudos

Same code from STM32L476RG won't run on one core of STM32H747.

On a my Nucleo-L476RG board, I used cube to only activate an LED connected gpio (PA5) - Nothing else.Then I programmed some blinky code into the main while loop:            HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, RESET);           HAL_Delay(1000);     ...

PAngl.14 by Associate II
  • 1721 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.