STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Circular DMA bursts

I use circular DMA with a buffer of size n (on a G431) to create bursts that are not necessarily equal to a multiple of n in size. This works fine, I start and stop a timer and end up somewhere in the DMA buffer array (say, at buffer[m] where 0<=m<n)...

MarcelH by Associate II
  • 2881 Views
  • 5 replies
  • 0 kudos

I am trying to interface an stm32f412 with a Texas instruments ADS7953 in the auto 2 mode. I am using the TI mode and using the HAL DMA drivers to talk to the ADS7953. However after programming I am not getting the intended result.

As I understand it TI mode consists of high polarity clock, 1st edge phase and nss after every frame. I think the problem I have is the clock is running even with NSS high. This causes the bits to be shifted out of the ADS7953. It will be great if an...

NKoti.1 by Associate
  • 920 Views
  • 0 replies
  • 0 kudos

IR remote

I'm trying to code IR remote which uses NEC protocol using STM32f030 .I'm able to do the code under while(1) as as a GPIO input But i'm not able to implement it as an interrupt . Kindly help me regarding the same

OKuma by Associate II
  • 5472 Views
  • 12 replies
  • 0 kudos

Simulink target ADC not working for STM32F091

I am trying to use the ADC_Read block from the simulink support package. I am able to use the ADC1 from a STM32F4 MCU but when I try to use the ADC from STM32F0 MCU it doesn't work. All the configurations should be fine since many other blocks work (...

jagjordi by Associate
  • 763 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.