STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Step Signals at The Conversion Output of The ADC

Hello,I use internal ADC of the STM32F767 microprocessor. When I plot the converted data in the Excel, I see a step signals initially. But when I check the analog signal input of the ADC with oscilloscope, there is no signal as step signals initially...

AE104 by Senior
  • 2835 Views
  • 5 replies
  • 0 kudos

How best to connect multiple memories

Hi,I am working on a fairly complex setup. I have a need for a fair bit of SDRAM and also potentially a lot ofstorage. So i would like to use NAND FLASH. I also have some small QSPI memory for system profiles and firmware updates etc.My MCU is the ST...

CEagl.1 by Associate III
  • 1210 Views
  • 1 replies
  • 0 kudos

I2c HAL_I2C_ERROR_AF error in slave mode

Hello,I am using I2C on STM32F part STM32F407VG.I have taken example code from https://github.com/PaxInstruments/STM32CubeF4/tree/master/Projects/STM32F4-Discovery/Examples/I2C/I2C_TwoBoards_ComITThe I2C configuration for STM32F as slave are followin...

MAbba.2 by Associate II
  • 1606 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G4 ADC clock frequency limitations

Hi,I would like to get some clarification on the maximum STM32G4 ADC clock frequency. In the STM32G473xB datasheet (DS12712 Rev 2), on page 138 it shows a max fADC of 60 MHz for Range 1, single ADC operation. What exactly is meant by "single ADC oper...

galens by Associate II
  • 5167 Views
  • 7 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.