STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can I find the end of memory in a bin file?

Hello,Currently, the generated binary file is 1 MB but with 96% of '0'.Obviously, it's quite long to transfer via CAN to update the firmware, mostly for 'nothing'.I can see that the 'end' of my code is: 1000 0000 0100 0000 4078 7d01 0000 0000Is it...

ABonn.1 by Associate
  • 2842 Views
  • 4 replies
  • 0 kudos

Resolved! Timer initialisation to *not* set the ARPE bit ?

I would like to know what is the correct way to disable a timer’s ARR preload function using the HAL library ? And once that’s done, does the ARPE bit stay low for the whole runtime, or does it have to be cleared again regularly or after specific eve...

pr by Associate III
  • 2852 Views
  • 4 replies
  • 0 kudos

Resolved! Differential signal test via boundary scan test

I want to test differential signal on STM32F407VG discovery board using boundary scan testing. I know that this soc supports boundary scan testing but is it possible to test/measure differential signal also via same way?

Rsrma.1 by Associate III
  • 3941 Views
  • 9 replies
  • 0 kudos

How to use SPI + DMA with software CS?

Hi All, I am trying to use SPI+DMA in stm32f401 nucleo 64. SPI + DMA is working successfully on both transmit and receive data. I configured spi + dma in software cs since I have multiple slaves, but that means I have to pull the gpio up and down for...

jb by Associate II
  • 4803 Views
  • 5 replies
  • 0 kudos

UART NOT Transmit if there is a delay in while loop

Hi, I generated the code through CUBEMAX, using USART3 with DMA and trying to send couple of bytes by call HAL_UART_Transmit_DMA in main while(1) loop. If I add the delay after a transmission even a 1ms it stop transmitting but if I remove the delay ...

ARehm by Associate III
  • 1818 Views
  • 2 replies
  • 0 kudos

STM32F767 - low power detection

In STM32F7 controller is there a way to detect low power mode in software and how long controller will work before it completely shuts off.

AShel.1 by Associate III
  • 1407 Views
  • 2 replies
  • 0 kudos

Resolved! I'm falling in a hardfault with the STM32F405VG during a ST routine "HAL_SPI_Transmit". Can you help me please ?

Hi everyone,First, my program was running good since many weeks and last week I added some code and from this day, each run of my program, i'm falling in hardfault handler... all the time in "HAL_SPI_Transmit".First thing i've done is to increase (so...

0693W000003BaozQAC.png 0693W000003Bau4QAC.png 0693W000003BavqQAC.png 0693W000003BawKQAS.png
GLE B.1 by Associate II
  • 1559 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.