STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SetRange problem in X axis

Hello, I've wrote SetRange in a graph like SetRange(0, 50, 0, 50), but the problem is my graph is stretched an i want have it in a compressed look. So i changed it to setRange(0, 100, 0, 50), but my x axis was shorten to 1/4 and rest of my X axis rem...

MHaji.1 by Senior
  • 697 Views
  • 0 replies
  • 0 kudos

SD card write using SDIO (4 bit) with DMA enabled is making system fail. I suspect cyclic write of around 200 bytes at 100 Hz is leading to bus contention issue or so.

Am using sTM32F4 Discovery board with extension board for RS232 interface and SD card.RS232 is also using DMA and its priority is higher than that of SD card DMA channel priority. The tasks working on RS232 interface and SD card log are different to...

DevBee by Associate II
  • 653 Views
  • 0 replies
  • 0 kudos

Resolved! Reading from Accelerometer via i2c on STM32F3 Discovery

Can anyone tell me the difference between those functions:HAL_I2C_Master_ReceiveHAL_I2C_Mem_ReadThe problem with HAL_I2C_Master_Receive is that it accepts too few parameters (hi2c, DevAddress, pData, Size, Timeout).I don't know how to tell the memory...

Ala1980 by Associate II
  • 4319 Views
  • 5 replies
  • 0 kudos

Lots of ADC Noise with STM32F103RBT6 and STM32F103C8T6

Hello,i'm doing my first project with the STM32F103, where ADC is involved.I want to read out several potentiometers and send MIDI commands to a PC.So far everything is working, but there is soo much noise on the ADC data. I'm using only the upper 7 ...

JanGE by Associate
  • 2766 Views
  • 2 replies
  • 0 kudos

[STM32F072] Problem in use all 4 UARTs in same time

I am creating a hub to connect several devices together. When I send a frame to one of the UARTs from an external device, I get an interrupt from each of the UARTs instead of just the one I sent to. what i am doing wrong?I generated configuration in ...

Metya by Associate II
  • 1146 Views
  • 2 replies
  • 0 kudos

QSPI missing first nibble

HiI am using the STM32F723 to read FPGA with the (notorious) QSPI interface in a custom board.The QSPI is configured to indirect read mode, 4 bits, using DMA.The issue is that the first nibble is not read. All other bytes are as expected.The Errata s...

Arnon by Associate III
  • 2755 Views
  • 4 replies
  • 0 kudos

Resolved! Not getting interrupt on stm32L5

Hi ST Team,I have used STM32L562-edk EVK for code development. I have configured gpio as a interrupt pin. When Interrupt is generated I have not getting interrupt in ISR routine. I have validated pin using read the gpio and get as expected behavior. ...

Neel by Associate III
  • 6245 Views
  • 8 replies
  • 1 kudos

Resolved! STM32F411VET UART2 questions

Hi, I've some questions about STM32F411VET and UART2.Is UART2 in this MCU native or emulated?I ask this, because despite I use an interrupt to receive data through calling to "void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)" callback, I had t...

SDall.11 by Associate III
  • 2684 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.