STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can STM32F303 be programmed in multi-drop?

We have a system that uses hundreds of modules. Each module has 4 STM32F303 MCU's. Within a single module we would like to have one programming interface. Is there a means to program 4 MCUs with one programming interface?

BTrem.1 by Senior II
  • 1281 Views
  • 3 replies
  • 0 kudos

WRITING TO FLASH WITH UART

Hi everyone,I can write to flash of STM32F103, max value of uint32 variable 4294967294.It is possible to write when you write it to flash directly.But I want to write it to flash with uart receiving. But when I put the rows (which is writed Bold in c...

UUrcan by Associate II
  • 5240 Views
  • 9 replies
  • 0 kudos

HAL_UART_Receive Timeout

Hello,I'm trying to understand: When will the HAL_UART_Receive function return HAL_TIMEOUT ?Will it happen only when the "Timeout" value has passed ?/** * @brief Receive an amount of data in blocking mode. * @note When UART parity is not enable...

skon.1 by Senior
  • 4561 Views
  • 5 replies
  • 0 kudos

J14 on STM32H745IIK6 - VDD or VSS

There's an error either in the datasheet and CubeMX or in the IBIS and BXL files.In the datasheet and CubeMX, J14 pin on STM32H745IIK6 (UFBGA 176+25) is labeled as VSS, but in the BXL file (Altium SchLib) and in the IBIS file, it is labeled as VDD.Co...

DTomi.1 by Senior
  • 1058 Views
  • 1 replies
  • 1 kudos

Resolved! X-CUBE-AWS demo project on B-L4S5I-IOT01A does not run

I'm trying to run the aws_demos project from X-CUBE-AWS on the B-L4S5I-IOT01A development board. I've successfully programmed and run the provisioning image. I've successfully built the aws_demos project, and have the "B-L4S5I-IOT01_aws_demos.sfb" an...

CAN Bus DATA IS NOT GETTING RECEIVE NOT BY POLLING NOR Rx NOTIFICATION INTERRUPT ITS STUCKs IN TO "HAL_CAN_GetRxMessage(&hcan1,CAN_RX_FIFO0,&Rx_Header,Rx_Data);" if this receive API we are using polling mode instead of interrupt one

As per CAN new API i have implemented as followed sequence:-MX_CAN1_Init();CAN_filterConfig(); if (HAL_CAN_Start(&hcan1) != HAL_OK) { Error_Handler(); } if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_FULL |CAN_IT_TX_MAILBOX_EMPTY) != HAL_O...

Why Flash is not erased Properly using HAL API? What would be the flash value after erasing? should it return 0xFF?

I am working on STM32H743 series, and I want to do Write operation continuously. When the flash is erased by STM32CubeProgrammer it returns 0xFF, but after erasing with HAL API (HAL_FLASHEx_Erase()), I got the value other than 0xFF (i.e previously fl...

STura.1 by Associate II
  • 1289 Views
  • 2 replies
  • 0 kudos

STM32 I2C TXIS flag not set.

Hi I am using B-L072Z-LRWAN1 board and connected ToF sensor to I2C1 (PB8 and PB9).I am using the following I2C configuration: __HAL_RCC_I2C1_FORCE_RESET(); __HAL_RCC_I2C1_RELEASE_RESET(); I2cHandle1.Instance = ( I2C_Ty...

Problems using git with TouchGFX

Hello everyone,We are using git with TouchGFX so more than one developer can work in the same TouchGFX file. However every time we try to merge the project it get corrupted. We also tried to some the confiltc manually but it also didn't work.I would ...

FDigi by Associate III
  • 832 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.