STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Adapting Custom Keyboard GUI to multi-screen application

I have been fighting to get the keyboard adapted to a multi-screen application for several days. I have gone thru the code generated by the Custom Keyboard GUI and the code that I have adapted for my application. I just don't see how to get the keybo...

LDoyl by Associate III
  • 715 Views
  • 0 replies
  • 0 kudos

Problem with simple I2C read on STM32F105

I am simply trying to read a few bytes from an I2C memory device using the following code: uint8_t buff[ 4 ]; HAL_I2C_Mem_Read( &hi2c1, ( uint16_t )( 80 << 1 ), 0, I2C_MEMADD_SIZE_16BIT, buff, 4, 10 );However, when I look at the output on the ...

0693W000005ANzHQAW.png

Resolved! STM32F103RGT6 - Confusion about adc pins

Hello.I want to use ADC in my STM32F103RGT6 Uc, but I don't understand what pdf's says about where the pins are.In this document We can see, that there are 3 ADC converters: ADC1, ADC2, ADC3.However, reading further on page 29, I can see alternate fu...

fifi_22 by Associate III
  • 1337 Views
  • 1 replies
  • 0 kudos

Apparently a conflict when clearing TC flags of DMA2 Streams

Hello to all, I hope you and your families are safe and sound. I am working to improve my project based on the STM32F469 MCU, but now I am experiencing a weird behavior. I can't post the code of course, too many files connected, so I will try to expl...

Digimorf by Associate III
  • 5343 Views
  • 8 replies
  • 0 kudos

Resolved! concatenate 2 byte arrayes

hi there I want to concatenate these 2 byte arraysuint8_t START_BYTE[2]={0x05,0x64};and uint8_t disunsini[]={0x15,0x3C,0x02,0x06,0x3C,0x03,0x06,0x3C,0x04,0x06};so I can get {0x05,0x64,0x15,0x3C,0x02,0x06,0x3C,0x03,0x06,0x3C,0x04,0x06};I used the code...

Ala by Senior
  • 3753 Views
  • 1 replies
  • 0 kudos

Resolved! Wrong clock source on Timer!

Hello,I am trying to program my TIM2 to set an interrupt every 100ms. As seen in the pictured that is attached, its APB runs on 170MHz. Given so, I have set the prescaler to 34000 and the counter to 500.It has been functioning correctly this whole t...

PMach.1 by Senior
  • 2629 Views
  • 5 replies
  • 0 kudos

Product Service Life

Model Name: STM32F103RCDear Sir or Madam,Greetings from Korea.I’m a RA of a medical device manufacturer in Korea.I'm writing to ask about if you could provide any document which shows the product's service life.According to IEC 60601-1, Clause 4.4, w...

SWON.1 by Associate
  • 1197 Views
  • 1 replies
  • 0 kudos

How to choose the 8MHz crystal oscillator for STM32F407?

I'm trying to replace the oscillator of the STM32F407 since I can't find anywhere the one listed in the bill of materials:It's a 8Mhz crystal oscillator from jfvny and it is in a HC-49/S package, the load capacitance is 20pF and frequency tolerance o...

0693W000005AKunQAG.png 0693W000005AKuOQAW.png
SFara.1 by Associate
  • 4780 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F072RB HSE/32 RTC calibration

Hi,l'm using the STM32F072RB for a programmable periodic wakeup of a system. I have some troubles in the RTC calibration. I have a 8MHz crystal oscillator connected to HSE and, since I won't put in stop/standby mode the mcu, I would like to use it as...

FCope.1 by Associate II
  • 4626 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.