STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer implementation

I am using STM32F072RB.On my system there is 5 buttons(which is connected to GPIO).I am reading that GPIO continuously to detect the button press.If there is no any button press detect for 10 min, I want to generate a alarm. And if any of the button ...

Bs.1 by Associate II
  • 1057 Views
  • 2 replies
  • 0 kudos

Boot configuration for STM32G071

For STM32G071 controller, I see difference in information provided in Ref manual (RM0444 Rev4) and STM32 microcontroller system memory boot mode applicate note(AN2606 Rev44).In Ref manual on Pg 60 section 2.5 it is mentioned that for selecting boot f...

0693W000006EagAQAS.jpg 0693W000006Eag5QAC.jpg 0693W000006Eag0QAC.jpg
AShel.1 by Associate III
  • 3182 Views
  • 5 replies
  • 0 kudos

Resolved! ADC(VDDA) Input Volatge

Hi,I am not quite sure about this. I have a STM32L100 µC operating at 1.8V, the analog pin sees a 3.0V coming from a battery and I want to use the ADC to be able to monitor the voltage of the battery.I plan to supply the VDDA Pin with 3.3V (the VRef+...

How to debug without using a microcontroller ?

Hello, I would like to be able to run a program without using a board. I would like to be able to do continuous integration with Jenkins but I haven't found any solutions to emulate my STM32L072. Someone would have any idea ?

JorisS by Associate
  • 1243 Views
  • 1 replies
  • 0 kudos

PVD STM32L071

Dear,I use STM32L071 powered from serial 2xAA 1.5 V battery (3 Volts). I intended to use PVD to reset mcu when the VCC is dangerously low, but the lowest threshold to activate PVD IRQ is 1.9 V. Problem is that for me is shame to reset whole MCU at 1....

JJRR by Senior
  • 873 Views
  • 2 replies
  • 0 kudos

Interfacing 4-bit SDIO with STM32L452 Nucleo board

Hi,I am trying to interface 4-bit SDIO with STM32L452 Nucleo board.So far, I have tried CubeMx and SDFAT library, but it doesn't seem to work.I have tried same interfacing and library with other variants(STM32F407) and its working fine.Is there any i...

AKuma.24 by Associate
  • 1329 Views
  • 2 replies
  • 0 kudos

SD card is always in 'TRANSFER' state.

HiI'm using STM32F103VGT6 and now days i have a problem in working with SD cards.I can't use FatFs library."HAL_SD_GetCardState" function, always return 'TRANSFER' state.I try multiple SD cards, clock divider and any many configs.please help.thanks

ENo.1 by Associate II
  • 3421 Views
  • 6 replies
  • 0 kudos

How do I get data out of an ISR safely?

I've been making decent progress on learning how to use C/C++ to replace an existing C# embedded application. I've cut a few corners along the way and I'd like to see if I can clean up the worst ones. Right now I have an ISR getting pressure data f...

magene by Senior II
  • 2559 Views
  • 6 replies
  • 0 kudos

Resolved! STM32G431KB Nucleo Board A2 not connected to PA3

I have been spending a few hours debugging my STM32G431KB Nucleo USART2 Rx not working and have found that the chip pin PA3 is not wired to the header A2 (or 11). Tx on PA2 (A7/5) works fine.Am I missing something? I ended having to solder a wire ...

DWalt.1 by Associate II
  • 1759 Views
  • 2 replies
  • 0 kudos

DFSDM with ADC not responding - STM32L562

Hello Community,I am trying to post-process my just sampled ADC values with the DFSDM sinc-Filter and mainly the oversampler.The problem ist: My DFSDM doesn't output anything. I tried DMA and polling. Polling generates a timeout.I configured the ADC ...

MPetr.3 by Associate III
  • 899 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.