STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to program STUSB4500 using NUCLEO STM32L4R5ZI?

We are using STUSB4500 in our custom board, as we are not having STM32F072RB Nucleo board with us we are using STM32L4R5ZI nucleo board which is available.I have downloaded STSW-STUSB004 for customizing the available library.I have STSW-STUSB004 ope...

Kpach.1 by Associate
  • 1140 Views
  • 1 replies
  • 0 kudos

IDE / toolchain for direct register access?

Hi. Any recommendations for an IDE and toolchain for a Nucleo board with STM32f3xx. I want to be close to the metal and would like to access registers directly example:TIMER1_BASE->CR1 |= 0X0001; // Start timerCapture[edge] = TIMER2_BASE->CCR1​;I wa...

RMalc.1 by Associate II
  • 1272 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F3xx Can the DAC be switched between multiple comparators?

Hi, I'm new here. Working with STM32F303 and wanting to use the DAC externally and internally with comparators in an adaptive threshold config. Can the DAC be disconnected and the COMP internal + point hold a charge and continue to work while the DAC...

RMalc.1 by Associate II
  • 1729 Views
  • 2 replies
  • 0 kudos

What is the purpose of the U7 op amp on Nucleo-144 boards?

Hi, as the title asks. On my STM32F767 Nucleo board, there is an Op Amp U7 (TSV631AILT) that buffers user LD1 connected to a pin (either PB0 or PA5). What is the purpose for this? I'm sure it's obvious but it's not standing out to me and there's no ...

0693W000007BgMYQA0.png
CDyer.1 by Senior
  • 1277 Views
  • 2 replies
  • 1 kudos

Resolved! Preserving SPI data in DMA circular mode

I'm trying to establish communication between a Raspberry Pi and an STM32F407. The Pi is Master and the F407 is a full duplex slave. The SPI is configured with circular mode DMA. When the data is sent from the Pi, I do receive it at the F407. However...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.