STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Does the STM32 v1.5.1 GCC 7.3.1 toolchain have a limitation of 32-bit arguments for variable argument lists (stdarg.h) ? I am trying to pass 64-bit arguments via a variable argument list and I only see the upper 32-bits set (lower 32-bits are zero).

I'm using the standard ANSI va_args approach here: int64_t arg64 = va_arg(args, int64_t);When stepping through the code the debugger clearly shows me a value like: 0xbeefbeef00000000

MNeed.1 by Associate
  • 1327 Views
  • 2 replies
  • 0 kudos

high baud rates dropping carachters

hi i'm using the stm32h750 and in it using the baud rate of 500000 well i want ot go higher but everytime i increase the baud rate there is some charachters dropped or missing in the final received message i tried DMA its worst not filling the buffe...

bakhti by Associate II
  • 4446 Views
  • 16 replies
  • 0 kudos

Different ways(syntax) to write resgisters in Keil IDE

Hi all, i saw someone use a different way to write instructions in keil IDE , where they would write something similar to what i tried to do in the photo.i usually would write which workis just fine , any ideas how to write what im trying to ?

AMat.1 by Associate II
  • 1107 Views
  • 1 replies
  • 0 kudos

Write data to flash when power supply drops

Hello,I am using a STM32G473VET6 on my board, and I want to save a few data bytes in Flash when the 24V power supply drops. I have more than 400ms available between the detection by the MCU and the 3.3V dropping. When the ADC triggers this event, the...

ATurp.11 by Associate II
  • 9595 Views
  • 22 replies
  • 0 kudos

Resolved! Copy input pin to output.

What would be an efficient, low latency way to reflect the state of an input pin onto an output pin?Is there anything more automated than configuring the input pin as an EXTI, then in the interrupt handler, reading it and setting the state of the out...

BCoch by Senior
  • 7306 Views
  • 12 replies
  • 0 kudos

SD Bus speed mode

Hello,as I see at the AN5200 only in DS and HS the signal level is 3.3V.Does it mean that the IO signal level in SDR50 for example will be 1.8V on the host side?The MCU has internal LDO for it ?Or the host size is always 3.3V, and the signal voltage ...

Pkats.1 by Associate II
  • 3747 Views
  • 2 replies
  • 0 kudos

ADC DMA Double / Multiple Buffer Example

Hello,I was searching in every STM32 CubeMX pack examples for ADC DMA with Double / Multiple Buffering. But I found nothing.I found in dma_ex hal file the functions like HAL_DMAEx_MultiBufferStart (or HAL_DMAEx_MultiBufferStart_IT), but they aren't u...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.