STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H755, IPCC

In my project I have to share some info among the two cores in the STM32H755 controller but I'm not able to find some simple example about the use of IPCC. Yes, there are presentations etc, but STM32Cube_FW_H7_V1.8.0 repository doesn't provide one.

JTeba.1 by Associate
  • 970 Views
  • 1 replies
  • 0 kudos

Resolved! FDCAN callback function is not called

Hello,I am trying to set up a FDCAN communication between two STM32G431KBT6.The Tx part seems to work perfectly but I have a problem at the level of the reception.General informations: I use CAN-FD as a standard CAN 2.0B (Extended Id) at a baud rate ...

alxrey by Associate II
  • 4609 Views
  • 1 replies
  • 3 kudos

Resolved! NUCLEO-L476RG access SD card using SPI

Dear allI am trying to access my SD card using SPI, I tried the code below but I couldn't get it work.is there any official tutorial about SD card of NUCLEO-L476RG?SD CARD Info: 32GB, SDHC, FAT formathttps://github.com/eziya/STM32_SPI_SDCARD

XZhen.2 by Associate II
  • 1537 Views
  • 1 replies
  • 0 kudos

STM32F0x1 Reference Manual (RM0091 Rev 9) does not specify what the values of USART ISR TEACK and REACK bits mean when they are 0 or 1.

Compare to other bitfields, e.g., :RWU0: Receiver in active mode1: Receiver in mute modeThere is no such 0 or 1 specified for TEACK and REACK bits.Also, discussion in USART Transmitter and USART Receiver sections do not discuss this.Thanks

Resolved! STM32 won't start without physical reset.

Hi, My mcu is STM32L476RGTx and I experiencing very strange behaviors to make my cpu start. This mcu is on pcb I designed myself.My boot0 pin is shorted to GNDAnd the reset pin pulled up to VCC.I can program my chip with my st link (updated to the la...

dodonny by Associate III
  • 11535 Views
  • 19 replies
  • 0 kudos

Nucleo-L476RG - SD card not creating any .txt files or any files at all. Does anyone have an example code to let the sd card work ?

Hey guys,I am pretty new to stm32 (-> beginner) and I am trying to create a .txt file on my sd card. My pc is connected by usb to the Nucleo-L476RG board, which is connected to an onboard sd card.These are the connected pins:   /**SDMMC1 GPIO Configu...

TNguy.9 by Associate II
  • 6182 Views
  • 12 replies
  • 0 kudos

Undefined reference to HAL_UART_Init

Anyone knows how to fix undefined reference to HAL_UART_Init,HAL_UART_receiveI included all necessary files for this but somehow it doesn't find any reference#include "stm32f4xx_hal.h" #include "stm32f4xx_hal_conf.h" #include "usb_device.h" #include ...

arduo by Senior
  • 13077 Views
  • 11 replies
  • 1 kudos

How to use USART RTO timeout?

I have a STM32L4xx series microcontroller. My goal is to use RTO in USART to issue a timeout, from the time a read was attempted (not only from the last stop bit). This is needed as its possible for nothing to be received. How do I acheive this using...

Accessing outside flash area is working...

Tested to flash a 128k (STM32F105) device with a firmware (40k) that is compiled for 256k and it works. Even when the firmware reads and writes data (config) to address location 0x0083E000 which is way out of the 128k device memory area.Is there some...

HHaga.1 by Associate
  • 1501 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.