STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to manually enabling NVIC irq for timer6 in STM42F407

Hello, i have written the following code for interrupt delay based on timer as shown in the attached fileBut Keil shows the error bellow on the line.Why it gives me such error,how do i manually enable the IRQ of TIM6?Thanks, NVIC_EnableIRQ(TIM6_IRQ...

Nbkjh.1 by Associate II
  • 3331 Views
  • 3 replies
  • 2 kudos

Hi, I have the board and not received any confirmation

 Hi, I have the board and not received any confirmation (teams invitation) or confirmation, just the initial email. I have emailed tilen.majerle@st.com from the company email account but have gotten no response. I tried to book again however your sys...

Ahmed by Associate III
  • 1139 Views
  • 1 replies
  • 0 kudos

Resolved! How accurate is ST VREFINT Calibration?

I am using STM32F030F4P6. VREFINT is supposed to be calibrated at 3.3v +/- 10mV and 30 degrees C. In my application the VREFINT calibration value is 1543 meaning the reference voltage is 1.243V (3.3/4096*1543) this is on the high end of the spectru...

mp035 by Associate III
  • 12000 Views
  • 12 replies
  • 2 kudos

Why Usart2 data not recognised over FTDI transmition

Hello,I am trying to use USART2 TX-PA2 RX-PA3 with 115200 baudrate no parity as shown in the cubeMx settings.'u' in binary is 01110101's' in binary is 01110011I have generated the code bellow. and i got a photo of the scope signal as shown bellow....

0693W000007ZtZxQAK.jpg 0693W000007ZtiGQAS.jpg 0693W000007Zu1mQAC.jpg
Nbkjh.1 by Associate II
  • 1360 Views
  • 2 replies
  • 0 kudos

Resolved! Syntax of startup_stm32g030xx.s

Good afternoon,Maybe is an obvious question.I'm studying the default startup_stm32g030xx.s, a part of the syntax is figured out in the program manual of MCU and another part in the GNU AS command page.But, for example, those following commands: .synt...

RCave.1 by Associate
  • 1478 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.