STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32l475RC - TIM3 configuration when running in low power mode

Hi,in my Project I need a millisecond timer. Therefore I try to use TIM3. Now I have the following problem.For example, when the MCU runs in Run-Mode at 80 MHz TIM3 fires every 1 ms according to its configuration. But when the MCU runs in low power m...

mcoc7n by Associate II
  • 1287 Views
  • 2 replies
  • 0 kudos

How many times write flash memory with stm32f103c8

Now I am using stm32f103c8 and i'd like to write flash directly in launch periodSo I did make it write erase and read data using Hal_functions as you can see under/* * sjk_flash.c * * Created on: 2021. 4. 21. * Author: sungjinkim */     #i...

SKim.1761 by Associate III
  • 1916 Views
  • 2 replies
  • 0 kudos

HCLK and SYSCLK and Cortex-M Core speed

Hi. I am a little bit confused after reading Reference Manual.What is the difference beteen HCLK and SYSCLK?Which clock is used to feed MCU Core?When we talking about time to execute instruction which clock cycle does it concern?

sholojda by Associate III
  • 11664 Views
  • 8 replies
  • 0 kudos

How to send a message over the bus between 2 STM32F1?

Hi, I am working on a project and i have two stm32f1038ct6 blue pills and I have to send a message over the bus and verify that it was received properly. Any help would be appreciated =)We are using the stm32IDEWe are using stm32 Cube programmerWe ar...

GMump.1 by Associate
  • 1101 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.