STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BOOT0 pin and SWCLK pin are the same pin - Is that OK?

Hi!I'm using STM32G030F6P6 TSSOP-20 and I notice that BOOT0 pin and SWCLK pin are the same pin. If I want to program the STM32G030F6P6 MCU, then I only need SWDIO and SWCLK and NRST pin and forget about the BOOT0 pin because BOOT0 pin is not avaiable...

0693W00000BadcFQAR.png
DMårt by Lead
  • 4075 Views
  • 6 replies
  • 0 kudos

Resolved! STM32F042G6 CAN TX & RX example.

* I am using STM32F042G6,*I need examle for CAN Bus both TX & Rx,*Receive mode of (Interrupt)*i am using cube ide:4.24.0

Ss.61 by Associate III
  • 1633 Views
  • 3 replies
  • 0 kudos

SAI or SPI clock requirement as I2S slave

When acting as I2S master, the kernel clock frequency for SAI or SPI must be set to some multiple of the audio sample rate, and the bit clock and frame sync signals are then generated by dividing the kernel clock. Now, if acting as I2S slave the bit ...

HWidj.2 by Associate III
  • 1921 Views
  • 2 replies
  • 0 kudos

SPI always calling callback

Hello to everyone. I'm creating a project where i need to communicate via SPI. My main board, is configured as full duplex Master, and i have other STM working as full duplex slave. But, i have a problem. If i configure the boards to just have one fu...

IRodr.2 by Associate II
  • 3449 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.