STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Trying to make a Queue module for multiple UARTs

Hi gang. My application uses from 0 to 3 UARTs, or maybe USB CDC instead ... LOTS of end-user settable options. Even before I get to that, I'm not happy with my queue implementation that's to be used with UART (or CDC) Tx and Rx. I would love for th...

Grant Bt by Senior II
  • 3905 Views
  • 6 replies
  • 1 kudos

Why SPI returns busy after a while of sending correctly?

Hello ST community,I use a STM32F767ZI-Nucleo. There is a timer generating interrupts every 20ms. If a timer interrupt occurs I use HAL_SPI_Transmit_DMA to send some data. I monitor the return value of this function and after some time of sending wit...

LBaum.3 by Associate II
  • 22529 Views
  • 12 replies
  • 0 kudos

Custom board using STM32L053C8T6

Hi All I am trying to build a custom board (for the first time :)) using an STM32L053C8T6. The board will power an LED and do short burst measurements of its reflection off a strip (< 1s). I am trying to power up the board using a photovoltaic cell a...

NSoin.1 by Associate II
  • 2307 Views
  • 6 replies
  • 0 kudos

STM32F746 FMC configuration

Using STM32F746, I want to access Intel's 10AX032H2F35I2SG FPGA.During FMC Configuration, I do not know how to calculate and write the following parameters.I've seen the RM0385 documentation, but I don't know how to calculate it.I have to do it by to...

0693W00000BbcYEQAZ.png
Psang.1 by Associate
  • 1057 Views
  • 1 replies
  • 0 kudos

STM32L4R5 || Flash internal read/erase

Hello everyone,Dev Board based on STM32L4R5I am just trying to erase and then write something on the internal FLASH.I am trying to follow the example: https://github.com/STMicroelectronics/STM32CubeL4/blob/master/Projects/NUCLEO-L4R5ZI/Examples/FLASH...

POval.1 by Associate II
  • 3113 Views
  • 5 replies
  • 0 kudos

How to send data via CANFD from stm32H753AI to PC?

Hello,i am pretty new to this topic. I want to send simple data via CANFD from the stm32H/53AI to a PC. For that i have the CANFD-USB adapter from PEAK and to display the data i am using PCAN-View. I discovered the function and i put in the addresses...

0693W00000BZdZiQAL.png
PHumm.1 by Associate
  • 1876 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.