STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Does it exist any SPL library for stm32f7 or not? and how can I switch to stm32f7 without using HAL library?

I have a project on stm32f4 with SPL library(standard peripheral library), so I want to switch to stm32f7 mcu and now i want to know is there any SPL library for stm32f7. i couldn't switch to hal library so is stm has any life time code for it or not...

HMogh by Associate
  • 1523 Views
  • 2 replies
  • 0 kudos

MCU upgraded from STM32F103 to STM32L475. Facing issue in ADC part. In the F103 MCU ADC clock derived from HCLK and to meet the same sampling time we used ADC clock PLLSAI1 in L475.

The issue is that at the normal conditions we are able to read the ADC values properly and when we put our device in the field then we are facing noise issues in ADC values. When we put old MCU no noise issue is coming but when we put new MCU then no...

Harish1 by Associate III
  • 1284 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F030xx hitting random Hardfaults

Hi guys,I hope you can help me with this one:In approximately 1 out of 100 devices we have some strange behaviour which ultimately boils down to a HardFault Interrupt which triggers a Watchdog Reset.The majority of products in the field does not have...

There is an error when i debug my code in the stm23CubeIDE.

When I go to debug, there is an error saying some source file isnt found (__lib_init) or something like this. I dont remember the name exactly. Then it gives me an option to go to preferences. Also, the debug doesnt run properly, my peripheral regist...

KP.3 by Associate II
  • 1105 Views
  • 1 replies
  • 0 kudos

Resolved! Is STM32-product-family dead?

no distributor nor STM's eshop has any STM32-device."Out of stock" or "on allocation".Why shall we waste any further development time on STM32 when there are no chips available?So, is STM32 dead?In my opinion, STM32 is dead.Currently any other experi...

SEam72 by Associate II
  • 3627 Views
  • 5 replies
  • 1 kudos

RM0091 - is FLASH prefetch after reset on or off?

In RM0091, rev.9, 3.5.1 Flash access control register (FLASH_ACR):Reset value: 0x0000 0000[...]Bit 4 PRFTBE: Prefetch buffer enable 0: Prefetch is disabledIn RM0091, rev.9, Prefetch controller  within 3.2.1:After reset, the state of the prefetch buff...

STM32L073RZ Low Power Standby mode

Hi Everyone,I am using stm32l073rz board, used both wakeup pin PWR_CSR_EWUP1 (PA0) and PWR_CSR_EWUP2 (PC13) for generating an interrupt to wakeup from standby mode, and I am enable both pin PWR->CSR |= (PWR_CSR_EWUP1 | PWR_CSR_EWUP2); before go to st...

Myada.1 by Associate II
  • 2796 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.