STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! A problem about the I2C Fast mode plus of STM32H750VBT6

I configured SYSCLK to 480 MHz and set the I2C1 peripheral clock frequency to 120 MHz. For I2C1's timing settings, I selected Fast Mode Plus (1 MHz) and applied the timing register value 0x0050174F, the setting about maximum output speed of SDA and S...

PKB404 by Associate
  • 689 Views
  • 2 replies
  • 1 kudos

Resolved! STM32N6 unused XSPI pins

Hi all,I'm designing STM32N655L0 based board and I've one question.I'm using XSPI1 and XSPI 2 peripherals.XSPI2->Octa SPI mode, NOR FlashXSPI1-> SDRAM, Hexa SPISo my question is can I use unused CS, NCLK pins as an IO?I just wanted to be sure. BR

batuhanky by Associate III
  • 484 Views
  • 1 replies
  • 1 kudos

NPU SRAM

Hi,I want to increase the amount of RAM for my application, but I noticed that the NPU seems to be using memory from address 0x34100000 (SRAM2) in the sample application it is based on. Where can I change this? Are there any limitations to the memory...

Artur5 by Associate III
  • 963 Views
  • 1 replies
  • 0 kudos

Resolved! Clock confirmation in NUCLEO-F767ZI

Hello,I was looking into this wiki tutorial on setting up a UDP echo server by @mƎALLEm , and the clock configuration caught my eye and wanted to confirm a few things.On the nucleo board , the 8 MHz crystal (X3) is not soldered and the 8 MHz clock si...

ak52_0-1753853874258.png ak52_1-1753854095962.png
ak52 by Associate III
  • 625 Views
  • 3 replies
  • 2 kudos

COMP connects to TIM

I am using a STM32H723ZGT6. I am trying to Trigger an Input Capture on TIM1 Channel 1 by connecting to the output of the Comparator internally,but cannot get the TIM1 Configuration to fire the Input Capture Callback. I've turned on the input capture ...

smile by Associate II
  • 598 Views
  • 1 replies
  • 1 kudos

Capture mode stm32f4

Hello,I have an STM32F429 project with a 1PPS input (PA0) and a 10Mhz oscillator (PB3) a PWM output (PA1), I can't get a value in my Timer2 it's always at 0, I don't see where my mistake is, can someone help me?Attached file (.zip)Thanks you all.Séba...

PSEBA.1 by Associate II
  • 507 Views
  • 1 replies
  • 0 kudos

Resolved! Designing a custom board with STM32H725ZGT3

I designed a custom board using the STM32H725ZGT3. The references I followed include the datasheet, application note AN5419, and the STM32H745ZIT6 Nucleo board design, among others. After powering up the board, I was able to connect to it via ST-Link...

Ironman by Associate II
  • 773 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.