STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Zener Diode from 5V rail to VDD across the LDO?

In AN4899 it specifies that one should add a zener diode from the 5V rail to the 3.3V rail in order to have complete safety when using FT pins with 5V pull ups. Does anyone know what the specifications of the Zener diode should be (currents, resistan...

0693W00000Dnnx7QAB.png
DJC by Senior
  • 2480 Views
  • 2 replies
  • 0 kudos

Resolved! Powering up a 5 volt tolerant external pull up.

Does anyone have experience with 5V pull ups? do you have to power on the 5V source after the MCU is started?I'm running a STM32L431CBT6  with external 5 volt 10k pull-ups on the pins PB11,12,13,14,15 and PA1. (all flagged as FT pins)I've been able t...

DJC by Senior
  • 14874 Views
  • 12 replies
  • 0 kudos

SPI communication with DMA handler

Hi, I have implemented SPI communication using DMA and it works. When i receive different data than the mentioned protocol format then it hangs and i dont receive any more data and i have to reset the chip to get back the communication. Is there any...

RBV by Associate II
  • 1035 Views
  • 1 replies
  • 0 kudos

CAN rollover between FIFOs after overflow in pooling mode

Hi everyone!I'm working with STM32F303. I'm configuring the CAN peripheral with HAL libraries for pooling mode operation. I'm wondering if there is a method to check only the FIFO0 fill level and configure the peripheral to move FIFO1 messages into F...

RGalvez by Associate II
  • 801 Views
  • 0 replies
  • 0 kudos

Boot to RAM from SD card on STM32H7...

Greetings!I've got custom hardware running on an ST32H7. I'm trying to load an image from the sdcard into off-chip RAM for execution. RAM's at 0xC0000000, and I think I've set the MPU configuration correctly: // Region 2 is the external RAM MPU_InitS...

Shouldn't DMA_HandleTypeDef State be volatile?

Current structure is:typedef struct __DMA_HandleTypeDef { ... HAL_DMA_StateTypeDef State; /*!< DMA transfer state */ ... } DMA_HandleTypeDef;Interrupts can change the State value, but it's not volatile, so the co...

Delivery Time of STM32H743ZIT6

Hi, I would have a question regarding the lead time of the STM32H743ZIT6. We use the part in multiple boards in our platform which is currently in prototype stadium. Fro the next charges of PCBs we are trying to order some uControllers (STM32H743ZIT6...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.